public interface DeformationParameters extends TaggedObject
Post
objects.
ResultManager
to create an DeformationParameters
Post
object
Session.resultManager()
. Modifier and Type | Method and Description |
---|---|
Result.Complex |
complexCriterion()
Returns the complexity criterion.
|
Result.Component |
component()
Returns the result component that is used for deforming the model.
|
Result.DeformationScale |
deformationType()
Returns the type of scale used for deforming the model
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
BaseResultType |
genericType()
Returns the result type that will be used for deforming the model
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
boolean |
isReferenceNode()
Returns a value of true means the reference node will be used
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
double |
phaseAngle()
Returns the phase angle at which result will be evaluated and used for deformation.
|
int |
referenceNodeLabel()
Returns the node label which identifies the reference node used when deforming the model if
isReferenceNode() is set to true
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX7.5.2 |
double |
scale()
Returns the scale to be applied to the deformation value
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setComplexCriterion(Result.Complex complex)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setComponent(Result.Component component)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setDeformationType(Result.DeformationScale unit)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setGenericType(BaseResultType type)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setPhaseAngle(double angle)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setReferenceNode(boolean isReferenceNode)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setReferenceNodeLabel(int referenceNodeLabel)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setScale(double scale)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
printTestData, printTestData, tag, tagValue
BaseResultType genericType() throws NXException, RemoteException
NXException
RemoteException
void setGenericType(BaseResultType type) throws NXException, RemoteException
type
- NXException
RemoteException
Result.Complex complexCriterion() throws NXException, RemoteException
BaseResultType.complex()
the complexity criterion
defines which value is used for deformation(like Result.Complex.REAL
or Result.Complex.IMAGINARY
)
NXException
RemoteException
void setComplexCriterion(Result.Complex complex) throws NXException, RemoteException
complex
- NXException
RemoteException
double phaseAngle() throws NXException, RemoteException
BaseResultType.complex()
and the complexCriterion()
and setComplexCriterion(nxopen.cae.Result.Complex)
is set to
Result.Complex.PHASE_ANGLE
,
the Phaseangle will be used to evaluate the value of the complex result
NXException
RemoteException
void setPhaseAngle(double angle) throws NXException, RemoteException
angle
- NXException
RemoteException
double scale() throws NXException, RemoteException
NXException
RemoteException
void setScale(double scale) throws NXException, RemoteException
scale
- NXException
RemoteException
boolean isReferenceNode() throws NXException, RemoteException
NXException
RemoteException
void setReferenceNode(boolean isReferenceNode) throws NXException, RemoteException
isReferenceNode
- NXException
RemoteException
int referenceNodeLabel() throws NXException, RemoteException
isReferenceNode()
is set to true
NXException
RemoteException
void setReferenceNodeLabel(int referenceNodeLabel) throws NXException, RemoteException
referenceNodeLabel
- NXException
RemoteException
Result.Component component() throws NXException, RemoteException
NXException
RemoteException
void setComponent(Result.Component component) throws NXException, RemoteException
component
- NXException
RemoteException
Result.DeformationScale deformationType() throws NXException, RemoteException
NXException
RemoteException
void setDeformationType(Result.DeformationScale unit) throws NXException, RemoteException
unit
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.