Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementModifyOrderBuilder.Operation |
ElementModifyOrderBuilder.Operation.MIDNODE
changes the midnode option for a parabolic mesh to mixed, curved or linear
|
static ElementModifyOrderBuilder.Operation |
ElementModifyOrderBuilder.Operation.ORDER
changes the order of a mesh from linear to parabolic or vice versa
|
Modifier and Type | Method and Description |
---|---|
ElementModifyOrderBuilder.Operation |
ElementModifyOrderBuilder.operationType()
Returns the operation option
License requirements: None. |
static ElementModifyOrderBuilder.Operation |
ElementModifyOrderBuilder.Operation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementModifyOrderBuilder.Operation |
ElementModifyOrderBuilder.Operation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementModifyOrderBuilder.Operation[] |
ElementModifyOrderBuilder.Operation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementModifyOrderBuilder.setOperationType(ElementModifyOrderBuilder.Operation operationType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.