public static class ElementModifyOrderBuilder.Operation extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MIDNODE
changes the midnode option for a parabolic mesh to mixed, curved or linear
|
static int |
_ORDER
changes the order of a mesh from linear to parabolic or vice versa
|
static ElementModifyOrderBuilder.Operation |
MIDNODE
changes the midnode option for a parabolic mesh to mixed, curved or linear
|
static ElementModifyOrderBuilder.Operation |
ORDER
changes the order of a mesh from linear to parabolic or vice versa
|
Modifier and Type | Method and Description |
---|---|
static ElementModifyOrderBuilder.Operation |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementModifyOrderBuilder.Operation |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementModifyOrderBuilder.Operation[] |
values()
Returns an array that contains the values for this enum.
|
public static final ElementModifyOrderBuilder.Operation ORDER
public static final ElementModifyOrderBuilder.Operation MIDNODE
public static final int _ORDER
public static final int _MIDNODE
public static ElementModifyOrderBuilder.Operation valueOf(int value)
public static ElementModifyOrderBuilder.Operation valueOf(String name)
public static ElementModifyOrderBuilder.Operation[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.