public static class ResultsEnvelopeBuilder.Output extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CREATE_FIELD |
static int |
_EXPORT_RESULT_FILE |
static ResultsEnvelopeBuilder.Output |
CREATE_FIELD |
static ResultsEnvelopeBuilder.Output |
EXPORT_RESULT_FILE |
Modifier and Type | Method and Description |
---|---|
static ResultsEnvelopeBuilder.Output |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultsEnvelopeBuilder.Output |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultsEnvelopeBuilder.Output[] |
values()
Returns an array that contains the values for this enum.
|
public static final ResultsEnvelopeBuilder.Output EXPORT_RESULT_FILE
public static final ResultsEnvelopeBuilder.Output CREATE_FIELD
public static final int _EXPORT_RESULT_FILE
public static final int _CREATE_FIELD
public static ResultsEnvelopeBuilder.Output valueOf(int value)
public static ResultsEnvelopeBuilder.Output valueOf(String name)
public static ResultsEnvelopeBuilder.Output[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.