Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ResultsEnvelopeBuilder.Output |
ResultsEnvelopeBuilder.Output.CREATE_FIELD |
static ResultsEnvelopeBuilder.Output |
ResultsEnvelopeBuilder.Output.EXPORT_RESULT_FILE |
Modifier and Type | Method and Description |
---|---|
static ResultsEnvelopeBuilder.Output |
ResultsEnvelopeBuilder.Output.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultsEnvelopeBuilder.Output |
ResultsEnvelopeBuilder.Output.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultsEnvelopeBuilder.Output[] |
ResultsEnvelopeBuilder.Output.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ResultsEnvelopeBuilder.setOutput(ResultsEnvelopeBuilder.Output output)
Set output type from result envelope
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.