Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static ClearanceAnalysisBuilder.NumberOfCollections |
ClearanceAnalysisBuilder.NumberOfCollections.ONE |
static ClearanceAnalysisBuilder.NumberOfCollections |
ClearanceAnalysisBuilder.NumberOfCollections.TWO |
Modifier and Type | Method and Description |
---|---|
ClearanceAnalysisBuilder.NumberOfCollections |
ClearanceAnalysisBuilder.totalCollectionCount()
Returns the setting to determine whether one collection or two collections should be used.
|
static ClearanceAnalysisBuilder.NumberOfCollections |
ClearanceAnalysisBuilder.NumberOfCollections.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceAnalysisBuilder.NumberOfCollections |
ClearanceAnalysisBuilder.NumberOfCollections.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceAnalysisBuilder.NumberOfCollections[] |
ClearanceAnalysisBuilder.NumberOfCollections.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ClearanceAnalysisBuilder.setTotalCollectionCount(ClearanceAnalysisBuilder.NumberOfCollections totalCollectionCount)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.