public static class ClearanceAnalysisBuilder.NumberOfCollections extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE |
static int |
_TWO |
static ClearanceAnalysisBuilder.NumberOfCollections |
ONE |
static ClearanceAnalysisBuilder.NumberOfCollections |
TWO |
Modifier and Type | Method and Description |
---|---|
static ClearanceAnalysisBuilder.NumberOfCollections |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceAnalysisBuilder.NumberOfCollections |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceAnalysisBuilder.NumberOfCollections[] |
values()
Returns an array that contains the values for this enum.
|
public static final ClearanceAnalysisBuilder.NumberOfCollections ONE
public static final ClearanceAnalysisBuilder.NumberOfCollections TWO
public static final int _ONE
public static final int _TWO
public static ClearanceAnalysisBuilder.NumberOfCollections valueOf(int value)
public static ClearanceAnalysisBuilder.NumberOfCollections valueOf(String name)
public static ClearanceAnalysisBuilder.NumberOfCollections[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.