Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
Modifier and Type | Method and Description |
---|---|
Arrangement |
ComponentAssembly.activeArrangement()
Returns
the currently active
Arrangement for this ComponentAssembly
License requirements: assemblies ("ASSEMBLIES MODULE") Created in NX3.0.0 |
Arrangement |
ArrangementCollection.create(Arrangement templateArrangement,
String name)
Creates a standard
Arrangement , based on an existing standard Arrangement . |
Arrangement |
ArrangementCollection.createIsolated(Arrangement templateArrangement,
String name)
|
Arrangement |
ArrangementCollection.findObject(String journalIdentifier)
Finds the
Arrangement with the given identifier as recorded in a journal. |
Arrangement |
ArrangementsBuilder.selectedArrangement()
Returns the selected arrangement
License requirements: None. |
Arrangement |
Component.suppressingArrangement()
Returns
the
Arrangement that controls this component's
suppression state. |
Arrangement |
Component.usedArrangement()
Returns
the Arrangement used for this component.
|
Modifier and Type | Method and Description |
---|---|
Arrangement |
ArrangementCollection.create(Arrangement templateArrangement,
String name)
Creates a standard
Arrangement , based on an existing standard Arrangement . |
Arrangement |
ArrangementCollection.createIsolated(Arrangement templateArrangement,
String name)
|
void |
Component.establishIsolatedPositionOverride(Component parent,
Arrangement arrangement)
Ensures there is an isolated positioning override for the
Component in the given part of
the given parent. |
ComponentAssembly.SuppressedStateData |
ComponentAssembly.getSuppressedState(Component component,
Arrangement arrangement)
Gets the suppression state of the component in the given arrangement.
|
Expression |
ComponentAssembly.getSuppressionExpression(Component component,
Arrangement arrangement)
Gets the expression controlling the suppression of the component in the given
arrangment
License requirements: None. |
boolean |
Component.isPositioningIsolated(Arrangement arrangement)
Get whether positioning for the selected
Component is isolated in the specified
Arrangement . |
ErrorList |
ComponentAssembly.releaseSuppression(Component[] components,
Arrangement[] arrangements)
Release control of the suppression state of an array of components.
|
void |
ComponentAssembly.setActiveArrangement(Arrangement newArrangement)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
ComponentAssembly.setDefault(Arrangement arrangement)
Set the default
Arrangement for the given ComponentAssembly . |
void |
Component.setPositioningIsolated(Arrangement arrangement)
Set positioning for the selected
Component as isolated in the specified
Arrangement . |
void |
ArrangementsBuilder.setSelectedArrangement(Arrangement arrangement)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
Component.setUsedArrangement(Arrangement newArrangement)
Changes the Arrangement used for this component.
|
ErrorList |
ComponentAssembly.suppressComponents(Component[] components,
Arrangement[] arrangements)
Suppresses an array of components
License requirements: assemblies ("ASSEMBLIES MODULE") . |
ErrorList |
ComponentAssembly.suppressComponents(Component[] components,
Arrangement[] arrangements,
String expression)
Suppresses an array of components in all
Arrangement s in this ComponentAssembly
License requirements: assemblies ("ASSEMBLIES MODULE") Created in NX5.0.1 |
ErrorList |
ComponentAssembly.unsuppressComponents(Component[] components,
Arrangement[] arrangements)
Unsuppresses an array of components in this ComponentAssembly
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Modifier and Type | Method and Description |
---|---|
Arrangement |
PostProcess.captureArrangement(String arrangementName,
int animationStep)
Capture or update an arrangement from motion result of active solution.
|
Arrangement |
PostProcess.captureArrangement(String arrangementName,
int arrangementType,
int animationStep)
Capture or update an arrangement from motion result of active solution.
|
Modifier and Type | Method and Description |
---|---|
Arrangement |
ComponentPositioner.primaryArrangement()
Returns
the
Arrangement in which the
primary Network will solve. |
Modifier and Type | Method and Description |
---|---|
ComponentConstraint.DirectionToFixed |
ComponentConstraint.getDirectionToFixed(Component component,
Arrangement arrangement)
Get the
ComponentConstraint.DirectionToFixed value of the ComponentConstraint
given a component and an arrangement. |
boolean |
ComponentConstraint.getSpecificInArrangement(Arrangement arrangement)
Get the arrangement specific state of this
ComponentConstraint in the
specified Arrangement . |
boolean |
ComponentConstraint.getSuppressedInArrangement(Arrangement arrangement)
Get the suppression state of this
ComponentConstraint in the
specified Arrangement . |
void |
ComponentPositioner.setPrimaryArrangement(Arrangement arrangement)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
ComponentConstraint.setSpecificInArrangement(Arrangement arrangement,
boolean arrangementSpecific)
Set the arrangement specific state of this
ComponentConstraint in the
specified Arrangement . |
void |
ComponentConstraint.setSuppressedInArrangement(Arrangement arrangement,
boolean suppressed)
Set the suppression state of this
ComponentConstraint in the
specified Arrangement . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.