public class TextType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ARBITRARY
Specifies the default text defined in the master symbol
which can be modified in the custom symbol.
|
static int |
_CONTROLLED
Specifies the text defined in the master symbol as enumerated
set of values, one of which can be selected in the custom symbol.
|
static int |
_INTEGER
Specifies ther text defined in the master symbol as an integer
constrained between maximum and minimum value.
|
static int |
_LAST
Last enum value.
|
static int |
_MANDATORY
Specifies text defined in the master symbol which can't be
modified in the custom symbol.
|
static int |
_PARTIALLY_CONTROLLED
Specifies the text defined in the master symbol as enumerated
set of values, one of which can be selected or overwritten in the
custom symbol.
|
static int |
_REAL
Specifies ther text defined in the master symbol as an real
constrained between maximum and minimum value.
|
static TextType |
ARBITRARY
Specifies the default text defined in the master symbol
which can be modified in the custom symbol.
|
static TextType |
CONTROLLED
Specifies the text defined in the master symbol as enumerated
set of values, one of which can be selected in the custom symbol.
|
static TextType |
INTEGER
Specifies ther text defined in the master symbol as an integer
constrained between maximum and minimum value.
|
static TextType |
LAST
Last enum value.
|
static TextType |
MANDATORY
Specifies text defined in the master symbol which can't be
modified in the custom symbol.
|
static TextType |
PARTIALLY_CONTROLLED
Specifies the text defined in the master symbol as enumerated
set of values, one of which can be selected or overwritten in the
custom symbol.
|
static TextType |
REAL
Specifies ther text defined in the master symbol as an real
constrained between maximum and minimum value.
|
Modifier and Type | Method and Description |
---|---|
static TextType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TextType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TextType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TextType MANDATORY
public static final TextType ARBITRARY
public static final TextType CONTROLLED
public static final TextType PARTIALLY_CONTROLLED
public static final TextType INTEGER
public static final TextType REAL
public static final TextType LAST
public static final int _MANDATORY
public static final int _ARBITRARY
public static final int _CONTROLLED
public static final int _PARTIALLY_CONTROLLED
public static final int _INTEGER
public static final int _REAL
public static final int _LAST
public static TextType valueOf(int value)
public static TextType valueOf(String name)
public static TextType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.