Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static TextType |
TextType.ARBITRARY
Specifies the default text defined in the master symbol
which can be modified in the custom symbol.
|
static TextType |
TextType.CONTROLLED
Specifies the text defined in the master symbol as enumerated
set of values, one of which can be selected in the custom symbol.
|
static TextType |
TextType.INTEGER
Specifies ther text defined in the master symbol as an integer
constrained between maximum and minimum value.
|
static TextType |
TextType.LAST
Last enum value.
|
static TextType |
TextType.MANDATORY
Specifies text defined in the master symbol which can't be
modified in the custom symbol.
|
static TextType |
TextType.PARTIALLY_CONTROLLED
Specifies the text defined in the master symbol as enumerated
set of values, one of which can be selected or overwritten in the
custom symbol.
|
static TextType |
TextType.REAL
Specifies ther text defined in the master symbol as an real
constrained between maximum and minimum value.
|
Modifier and Type | Method and Description |
---|---|
TextType |
CustomSymbolTextData.textType()
Deprecated.
Deprecated in NX9.0.0. Use
MasterSymbolListItemBuilder instead. Use Annotations.BaseCustomSymbolBuilder#texts to query list of custom symbol texts.
|
static TextType |
TextType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TextType |
TextType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TextType[] |
TextType.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.