SpecifyCircuitBuilder Class¶
-
class
NXOpen.Tooling.
SpecifyCircuitBuilder
¶ Bases:
NXOpen.Builder
Represents a builder to be used to create specify circuit.
To create a new instance of this class, use
NXOpen.Tooling.SpecifyCircuitCollection.CreateBuilder
Default values.
Property Value KeepCircuit 0 Layer 251 UseSymbol 1 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ChannelColor | Returns or sets the circuit channel body color. |
CircuitColor | Returns or sets the circuit channel temperary body color. |
InletChannel | Returns the inlet channel. |
KeepCircuit | Returns or sets the option whether to keep the circuit displayed body. |
Layer | Returns or sets the layer value for the selected channels. |
OutletChannel | Returns the outlet channel. |
Tag | Returns the Tag for this object. |
UseSymbol | Returns or sets the value which specifies whether to add real component or not. |
Methods¶
Method | Description |
---|---|
CheckStatus | Check whether cooling circuit is finished or not. |
Commit | Commits any edits that have been applied to the builder. |
CreateCoolingFittingData | Creates the cooling fitting data object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCoolingFittingData | Gets the Cooling Fitting Data object. |
GetObject | Returns the object currently being edited by this builder. |
GetOneCircuit | Gets intersect cooling list value. |
InitializeCircuitSetData | Initializes the circuit set data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ChannelColor¶
-
SpecifyCircuitBuilder.
ChannelColor
¶ Returns or sets the circuit channel body color.
-------------------------------------
Getter Method
Signature
ChannelColor()
Returns: Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChannelColor(channelColor)
Parameters: channelColor (Id) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”)
CircuitColor¶
-
SpecifyCircuitBuilder.
CircuitColor
¶ Returns or sets the circuit channel temperary body color.
-------------------------------------
Getter Method
Signature
CircuitColor()
Returns: Return type: Id New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircuitColor(circuitColor)
Parameters: circuitColor (Id) – New in version NX8.0.1.
License requirements: ug_mold_design (“UG MOLD”)
InletChannel¶
-
SpecifyCircuitBuilder.
InletChannel
¶ Returns the inlet channel.
-------------------------------------
Getter Method
Signature
InletChannel()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.0.0.
License requirements: None.
KeepCircuit¶
-
SpecifyCircuitBuilder.
KeepCircuit
¶ Returns or sets the option whether to keep the circuit displayed body.
-------------------------------------
Getter Method
Signature
KeepCircuit()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepCircuit(keepCircuit)
Parameters: keepCircuit (bool) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
Layer¶
-
SpecifyCircuitBuilder.
Layer
¶ Returns or sets the layer value for the selected channels.
-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
OutletChannel¶
-
SpecifyCircuitBuilder.
OutletChannel
¶ Returns the outlet channel.
-------------------------------------
Getter Method
Signature
OutletChannel()
Returns: Return type: NXOpen.SelectBody
New in version NX8.0.0.
License requirements: None.
UseSymbol¶
-
SpecifyCircuitBuilder.
UseSymbol
¶ Returns or sets the value which specifies whether to add real component or not.
-------------------------------------
Getter Method
Signature
UseSymbol()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseSymbol(useSymbol)
Parameters: useSymbol (bool) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”)
Method Detail¶
CheckStatus¶
-
SpecifyCircuitBuilder.
CheckStatus
¶ Check whether cooling circuit is finished or not.
Signature
CheckStatus()
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
CreateCoolingFittingData¶
-
SpecifyCircuitBuilder.
CreateCoolingFittingData
¶ Creates the cooling fitting data object.
Signature
CreateCoolingFittingData()
Returns: the new NXOpen.Tooling.CoolingFittingData
instanceReturn type: NXOpen.Tooling.CoolingFittingData
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
GetCoolingFittingData¶
-
SpecifyCircuitBuilder.
GetCoolingFittingData
¶ Gets the Cooling Fitting Data object.
Signature
GetCoolingFittingData()
Returns: Return type: NXOpen.Tooling.CoolingFittingData
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
GetOneCircuit¶
-
SpecifyCircuitBuilder.
GetOneCircuit
¶ Gets intersect cooling list value.
Signature
GetOneCircuit(channels)
Parameters: channels (list of NXOpen.Body
) – the cooling bodyNew in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
InitializeCircuitSetData¶
-
SpecifyCircuitBuilder.
InitializeCircuitSetData
¶ Initializes the circuit set data.
Signature
InitializeCircuitSetData()
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”)
Validate¶
-
SpecifyCircuitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.