CoolingFittingData Class¶
-
class
NXOpen.Tooling.
CoolingFittingData
¶ Bases:
NXOpen.TransientObject
Represents the cooling fitting data in Add Channel Fitting Builder.
To create an instance of this object use
Tooling.ChannelFittingBuilder.CreateCoolingFittingData
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
AddFittingPoints | Add cooling fitting points to the fitting data. |
ClearFittingPoints | Clear cooling fitting points from the fitting data. |
Dispose | Dispose the part infomation to be cloned. |
Method Detail¶
AddFittingPoints¶
-
CoolingFittingData.
AddFittingPoints
¶ Add cooling fitting points to the fitting data.
Signature
AddFittingPoints(fittingPoint)
Parameters: fittingPoint ( NXOpen.Point
) – the fitting point to be added.New in version NX7.5.0.
License requirements: None.