SlugRetentionBuilder Class¶
-
class
NXOpen.Tooling.
SlugRetentionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.SlugRetentionBuilder
which is used to create the Slug Retention.To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateSlugRetentionBuilder
Default values.
Property Value AngularDimension.Value 5 OffsetDistance 5 RadiusDimension.Value 7 (millimeters part), 0.25 (inches part) New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AngularDimension | Returns the angular dimension |
OffsetDirection | Returns or sets the offset direction |
OffsetDistance | Returns or sets the offset distance |
PreviousWorkPart | Returns or sets the previous work part |
RadiusDimension | Returns the radius dimension |
RotateDirection | Returns or sets the rotate direction |
SelectComponent | Returns the select component |
SelectPoint | Returns or sets the select point |
SlugRetentionBooleanData | Returns the slug retention boolean data |
SlugRetentionFeature | Returns or sets the slug retention feature |
Tag | Returns the Tag for this object. |
TargetBodyForSubtract | Returns or sets the target body for subtract |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngularDimension¶
-
SlugRetentionBuilder.
AngularDimension
¶ Returns the angular dimension
-------------------------------------
Getter Method
Signature
AngularDimension()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
OffsetDirection¶
-
SlugRetentionBuilder.
OffsetDirection
¶ Returns or sets the offset direction
-------------------------------------
Getter Method
Signature
OffsetDirection()
Returns: Return type: NXOpen.Direction
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetDirection(offsetDirection)
Parameters: offsetDirection ( NXOpen.Direction
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetDistance¶
-
SlugRetentionBuilder.
OffsetDistance
¶ Returns or sets the offset distance
-------------------------------------
Getter Method
Signature
OffsetDistance()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetDistance(offsetDistance)
Parameters: offsetDistance (float) – New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
PreviousWorkPart¶
-
SlugRetentionBuilder.
PreviousWorkPart
¶ Returns or sets the previous work part
-------------------------------------
Getter Method
Signature
PreviousWorkPart()
Returns: Return type: NXOpen.Part
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PreviousWorkPart(previousWorkPart)
Parameters: previousWorkPart ( NXOpen.Part
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
RadiusDimension¶
-
SlugRetentionBuilder.
RadiusDimension
¶ Returns the radius dimension
-------------------------------------
Getter Method
Signature
RadiusDimension()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
RotateDirection¶
-
SlugRetentionBuilder.
RotateDirection
¶ Returns or sets the rotate direction
-------------------------------------
Getter Method
Signature
RotateDirection()
Returns: Return type: NXOpen.Direction
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateDirection(rotateDirection)
Parameters: rotateDirection ( NXOpen.Direction
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SelectComponent¶
-
SlugRetentionBuilder.
SelectComponent
¶ Returns the select component
-------------------------------------
Getter Method
Signature
SelectComponent()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX10.0.0.
License requirements: None.
SelectPoint¶
-
SlugRetentionBuilder.
SelectPoint
¶ Returns or sets the select point
-------------------------------------
Getter Method
Signature
SelectPoint()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectPoint(selectPoint)
Parameters: selectPoint ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SlugRetentionBooleanData¶
-
SlugRetentionBuilder.
SlugRetentionBooleanData
¶ Returns the slug retention boolean data
-------------------------------------
Getter Method
Signature
SlugRetentionBooleanData()
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX10.0.0.
License requirements: None.
SlugRetentionFeature¶
-
SlugRetentionBuilder.
SlugRetentionFeature
¶ Returns or sets the slug retention feature
-------------------------------------
Getter Method
Signature
SlugRetentionFeature()
Returns: Return type: NXOpen.Features.Feature
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SlugRetentionFeature(slugRetentionFeature)
Parameters: slugRetentionFeature ( NXOpen.Features.Feature
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
TargetBodyForSubtract¶
-
SlugRetentionBuilder.
TargetBodyForSubtract
¶ Returns or sets the target body for subtract
-------------------------------------
Getter Method
Signature
TargetBodyForSubtract()
Returns: Return type: NXOpen.Body
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetBodyForSubtract(targetBodyForSubtract)
Parameters: targetBodyForSubtract ( NXOpen.Body
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
Validate¶
-
SlugRetentionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.