InheritPmiPreferences Class¶
-
class
NXOpen.Preferences.
InheritPmiPreferences
¶ Bases:
object
Represents set of InheritPmiPreferences applicable to drafting views.
To obtain an instance of this class use
Preferences.ViewPreferences.InheritPmi
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CrosshatchPmiLightweightSectionView | Returns or sets the cross-hatch setting for the current inherited PMI Lightweight Section View |
InheritGdt | Returns or sets the Inherit GD and T option |
InheritPmiMode | Returns or sets the Status of inherit pmi mode. |
InheritPmiToDrawing | Returns or sets the Status of pmi inherited to drawing. |
Methods¶
Property Detail¶
CrosshatchPmiLightweightSectionView¶
-
InheritPmiPreferences.
CrosshatchPmiLightweightSectionView
¶ Returns or sets the cross-hatch setting for the current inherited PMI Lightweight Section View
-------------------------------------
Getter Method
Signature
CrosshatchPmiLightweightSectionView()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CrosshatchPmiLightweightSectionView(crosshatch)
Parameters: crosshatch (bool) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
InheritGdt¶
-
InheritPmiPreferences.
InheritGdt
¶ Returns or sets the Inherit GD and T option
-------------------------------------
Getter Method
Signature
InheritGdt()
Returns: Return type: NXOpen.Preferences.GdtOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritGdt(gdtOption)
Parameters: gdtOption ( NXOpen.Preferences.GdtOption
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
InheritPmiMode¶
-
InheritPmiPreferences.
InheritPmiMode
¶ Returns or sets the Status of inherit pmi mode.
-------------------------------------
Getter Method
Signature
InheritPmiMode()
Returns: Return type: NXOpen.Preferences.PmiOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritPmiMode(pmiOption)
Parameters: pmiOption ( NXOpen.Preferences.PmiOption
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
InheritPmiToDrawing¶
-
InheritPmiPreferences.
InheritPmiToDrawing
¶ Returns or sets the Status of pmi inherited to drawing.
-------------------------------------
Getter Method
Signature
InheritPmiToDrawing()
Returns: Inherit to drawing flag Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritPmiToDrawing(pmiOption)
Parameters: pmiOption (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)