GdtOption Enumeration¶
-
class
NXOpen.Preferences.
GdtOption
¶ Bases:
object
Represents the Inherit GD and T options Enum Members
Enum Member Enum Member Description None Does not inherit any GD and T display instances.InDrawingPlane inherit display instances of geometric tolerance features that are parallel to the drawing plane onto the drawing view.FromModelView inherit display instances of geometric tolerance features that exist in a particular modeling view (e.g. Top, Front, etc.).-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-