PmiOption Enumeration¶
-
class
NXOpen.Preferences.
PmiOption
¶ Bases:
object
Represents the Inherit PMI options Enum Members
Enum Member Enum Member Description None Does not inherit PMI.FromModelView Inherit PMI from the parent model view.InDrawingPlaneFromView Inherit PMI that are parallel to the drawing plane from the model view.InDrawingPlaneFromPart Inherit PMI that are parallel to the drawing plane from the entire part.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-