NXOpen.Positioning.ComponentConstraint |
Constraint for use in positioning assembly objects in NX. |
NXOpen.Positioning.ComponentConstraintGroup |
Constraint group which represents a group of component constraints in NX. |
NXOpen.Positioning.ComponentConstraintGroupBuilder |
Represents a NXOpen.Positioning.ComponentConstraintGroupBuilder builder |
NXOpen.Positioning.ComponentNetwork |
Network for use in positioning components in NX. |
NXOpen.Positioning.ComponentPositioner |
An instance of this class can be used to create :py:class:`NXOpen.Positioning.Constraint`s and associated objects. |
NXOpen.Positioning.Constraint |
Constraint for use in positioning objects in NX. |
NXOpen.Positioning.ConstraintCollection |
a collection of constraints |
NXOpen.Positioning.ConstraintReference |
ConstraintReference for use in positioning objects in NX. |
NXOpen.Positioning.DisplayedConstraint |
The displayed representation of a constraint, used for graphical display and to represent it in the Assembly Navigator. |
NXOpen.Positioning.DisplayedConstraintCollection |
a collection of displayed constraints |
NXOpen.Positioning.MatingConverter |
An instance of this class can be used to convert Mating Conditions to Assembly Constraints in its owning assembly or in child parts of its owning assembly. |
NXOpen.Positioning.Network |
Network for use in positioning objects in NX. |
NXOpen.Positioning.Positioner |
An instance of this class can be used to create :py:class:`NXOpen.Positioning.Constraint`s and associated objects. |