ConstraintAlignment Enumeration¶
NXOpen.Positioning.Constraint.Alignment is an alias for NXOpen.Positioning.ConstraintAlignment
-
class
NXOpen.Positioning.
ConstraintAlignment
¶ Bases:
object
Specifies alignment of directed geometries used in a constraint.
Enum Members
Enum Member Enum Member Description InferAlign Allow the solver to decide the alignmentCoAlign Directions are the sameContraAlign Directions are opposite-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-