ProxyOverrideObjectCollection Class¶
-
class
NXOpen.Mechatronics.
ProxyOverrideObjectCollection
¶ Bases:
object
Represents a collection of Proxy Override Object.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateBuilder | Creates a NXOpen.Mechatronics.ProxyOverrideObjectBuilder . |
CreateProxyObjectParameterBuilder | Creates a NXOpen.Mechatronics.ProxyObjectParameterBuilder @return |
FindObject | Finds the NXOpen.Mechatronics.ProxyOverrideObject with the given name. |
Method Detail¶
CreateBuilder¶
-
ProxyOverrideObjectCollection.
CreateBuilder
¶ Creates a
NXOpen.Mechatronics.ProxyOverrideObjectBuilder
.Signature
CreateBuilder(proxyObjectOcc)
Parameters: proxyObjectOcc ( NXOpen.NXObject
) – input occurrence of the proxy definition object or proxy override object. NULL_TAG is not allowedReturns: Return type: NXOpen.Mechatronics.ProxyOverrideObjectBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateProxyObjectParameterBuilder¶
-
ProxyOverrideObjectCollection.
CreateProxyObjectParameterBuilder
¶ Creates a
NXOpen.Mechatronics.ProxyObjectParameterBuilder
Signature
CreateProxyObjectParameterBuilder()
Returns: Return type: NXOpen.Mechatronics.ProxyObjectParameterBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ProxyOverrideObjectCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ProxyOverrideObject
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ProxyOverrideObject
.Returns: NXOpen.Mechatronics.ProxyOverrideObject
with this name.Return type: NXOpen.Mechatronics.ProxyOverrideObject
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)