ProxyOverrideObjectBuilder Class¶
-
class
NXOpen.Mechatronics.
ProxyOverrideObjectBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ProxyOverrideObjectBuilder
.To create a new instance of this class, use
NXOpen.Mechatronics.ProxyOverrideObjectCollection.CreateBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Attachment | Returns the attachment that is encapsulated in the proxy override object |
Context | Returns or sets the context part of the proxy override object |
HasAttachment | Returns or sets the flag for whether the proxy override object has an attachment |
ParameterList | Returns the parameter data |
ProxyObject | Returns the proxy object that is encapsulated in the proxy override object |
ProxyOverrideObjectName | Returns or sets the name of the proxy override object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ProxyOverrideObjectBuilderAttrBoolValue Enumeration | the value for the boolean option |
ProxyOverrideObjectBuilderAttrType Enumeration | the parameter attribute option. |
Property Detail¶
Attachment¶
-
ProxyOverrideObjectBuilder.
Attachment
¶ Returns the attachment that is encapsulated in the proxy override object
-------------------------------------
Getter Method
Signature
Attachment()
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Context¶
-
ProxyOverrideObjectBuilder.
Context
¶ Returns or sets the context part of the proxy override object
-------------------------------------
Getter Method
Signature
Context()
Returns: Return type: NXOpen.BasePart
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Context(context)
Parameters: context ( NXOpen.BasePart
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
HasAttachment¶
-
ProxyOverrideObjectBuilder.
HasAttachment
¶ Returns or sets the flag for whether the proxy override object has an attachment
-------------------------------------
Getter Method
Signature
HasAttachment()
Returns: Return type: bool New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
HasAttachment(hasAttachment)
Parameters: hasAttachment (bool) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ParameterList¶
-
ProxyOverrideObjectBuilder.
ParameterList
¶ Returns the parameter data
-------------------------------------
Getter Method
Signature
ParameterList()
Returns: Return type: NXOpen.Mechatronics.ProxyObjectParameterBuilderList
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ProxyObject¶
-
ProxyOverrideObjectBuilder.
ProxyObject
¶ Returns the proxy object that is encapsulated in the proxy override object
-------------------------------------
Getter Method
Signature
ProxyObject()
Returns: Return type: NXOpen.NXObject
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ProxyOverrideObjectName¶
-
ProxyOverrideObjectBuilder.
ProxyOverrideObjectName
¶ Returns or sets the name of the proxy override object
-------------------------------------
Getter Method
Signature
ProxyOverrideObjectName()
Returns: Return type: str New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ProxyOverrideObjectName(proxyOverrideObjectName)
Parameters: proxyOverrideObjectName (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
ProxyOverrideObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.