RenameLinkedPartModulePartBuilder Class¶
-
class
NXOpen.GeometricUtilities.
RenameLinkedPartModulePartBuilder
¶ Bases:
NXOpen.Builder
Represents a
Features.PartModule
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateRenameLinkedPartModulePartBuilder
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllAssociatedLinkedPartModulePartTags | Get all linked part module part tags associated with given main part. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetLinkedPartNameToBeSavedAs | Retrieve new name of linked part module part added earlier for Save As. |
GetObject | Returns the object currently being edited by this builder. |
SetLinkedPartNameToBeSavedAs | Add linked part module part tag and its new name to perform Save As along with its main part. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetAllAssociatedLinkedPartModulePartTags¶
-
RenameLinkedPartModulePartBuilder.
GetAllAssociatedLinkedPartModulePartTags
¶ Get all linked part module part tags associated with given main part.
This function will also load linked parts if they are not loaded.
Signature
GetAllAssociatedLinkedPartModulePartTags(mainPartTag)
Parameters: mainPartTag ( NXOpen.Part
) – the main part for which linked part module parts are to be queriedReturns: all associated linked part module parts Return type: list of NXOpen.Part
New in version NX9.0.0.
License requirements: None.
GetLinkedPartNameToBeSavedAs¶
-
RenameLinkedPartModulePartBuilder.
GetLinkedPartNameToBeSavedAs
¶ Overloaded method GetLinkedPartNameToBeSavedAs
GetLinkedPartNameToBeSavedAs(linkedPartTag)
GetLinkedPartNameToBeSavedAs()
-------------------------------------
Retrieve new name of linked part module part added earlier for “Save As”.
Signature
GetLinkedPartNameToBeSavedAs(linkedPartTag)
Parameters: linkedPartTag ( NXOpen.Part
) – the linked partReturns: new linked part file name Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Retrieve all linked part module parts and their associated new names.
Signature
GetLinkedPartNameToBeSavedAs()
Returns: new linked part file name Return type: list of str New in version NX9.0.0.
License requirements: None.
-------------------------------------
SetLinkedPartNameToBeSavedAs¶
-
RenameLinkedPartModulePartBuilder.
SetLinkedPartNameToBeSavedAs
¶ Overloaded method SetLinkedPartNameToBeSavedAs
SetLinkedPartNameToBeSavedAs(linkedPartTag, fileName)
SetLinkedPartNameToBeSavedAs(linkedPartTag, fileName)
-------------------------------------
Add linked part module part tag and its new name to perform “Save As” along with its main part.
Signature
SetLinkedPartNameToBeSavedAs(linkedPartTag, fileName)
Parameters: - linkedPartTag (
NXOpen.Part
) – the linked part - fileName (str) – new linked part file name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Add multiple linked part module part tags and their new names to perform “Save As” along with its main part.
Signature
SetLinkedPartNameToBeSavedAs(linkedPartTag, fileName)
Parameters: - linkedPartTag (list of
NXOpen.Part
) – the linked part - fileName (list of str) – new linked part file name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Validate¶
-
RenameLinkedPartModulePartBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.