NXOpen.Fields.DisplayPropertiesBuilder |
Represents a builder class for editing display properties of a NXOpen.Fields.Field |
NXOpen.Fields.ExportData |
Represents data for field export |
NXOpen.Fields.Field |
Represents an Field abstract class. |
NXOpen.Fields.FieldDomain |
Represents the Field Domains. |
NXOpen.Fields.FieldDomainCollection |
Provides methods for manipulating the field domains |
NXOpen.Fields.FieldEvaluator |
Represents a Field Evaluator which can be used to evaluate a NXOpen.Fields.Field . |
NXOpen.Fields.FieldExpression |
Represents the Field Expression class. |
NXOpen.Fields.FieldFormula |
Represents the Field Formula class. |
NXOpen.Fields.FieldLink |
Represents the Field Link class. |
NXOpen.Fields.FieldLinksTable |
Represents the Field LinksTable class. |
NXOpen.Fields.FieldManager |
Represents the manager class of the Fields |
NXOpen.Fields.FieldReference |
Represents an reference field |
NXOpen.Fields.FieldTable |
Represents the Field Table class. |
NXOpen.Fields.FieldVariable |
Represents the Field Variables |
NXOpen.Fields.FieldWrapper |
This class defines a value that is internally backed up by a field. |
NXOpen.Fields.ImportData |
Represents data transfer objectst for field import |
NXOpen.Fields.NameVariable |
This class stores the common name and measure for field variables. |
NXOpen.Fields.PathObjects |
Contains objects that define a lattice path |
NXOpen.Fields.PathObjectsList |
Represents a list of objects. |
NXOpen.Fields.ScalarFieldWrapper |
This class defines a scalar value that is internally backed up by a (optionally scaled) field or an expression. |
NXOpen.Fields.SpatialMap |
Represents the Field Domain Map |
NXOpen.Fields.SpatialMapBuilder |
Represents a NXOpen.Fields.SpatialMap builder |
NXOpen.Fields.VectorFieldWrapper |
This class defines a vector value that is internally backed up by a (optionally scaled) field or three expressions. |