FieldEvaluator Class¶
-
class
NXOpen.Fields.
FieldEvaluator
¶ Bases:
NXOpen.TaggedObject
Represents a Field Evaluator which can be used to evaluate a
NXOpen.Fields.Field
.Use
NXOpen.Fields.Field.GetFieldEvaluator
to obtain an instance of this classNew in version NX7.5.2.
Properties¶
Property | Description |
---|---|
InterpolationMethod | Returns or sets the interpolation method used when this table data is evaluated. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Delete | Delete this field evaluator; destroys the field evaluator and removes all references to it. |
Evaluate | Evaluate the Field at the specified independent variable NXOpen.Fields.FieldVariable values and return the values for the specified dependent variable. |
GetDependentVariables | Returns the dependent variables for this NXOpen.Fields.FieldEvaluator @return dependent variables for this NXOpen.Fields.FieldEvaluator |
GetIndependentVariables | Returns the independent variables for this NXOpen.Fields.FieldEvaluator @return independent variables for this NXOpen.Fields.FieldEvaluator |
SetIndependentVariableValues | Sets values at which the Field will be evaluated for this independent variable NXOpen.Fields.FieldVariable . |
Enumerations¶
FieldEvaluatorInterpolationEnum Enumeration | Interpolation type |
FieldEvaluatorInverseDistanceWeightingEnum Enumeration | Options for IDW (inverse weighted distance) interpolator |
FieldEvaluatorLinearLogOptionEnum Enumeration | Log Options for Linear interpolator |
FieldEvaluatorValuesOutsideTableInterpolationEnum Enumeration | Options for outside table values interpolation |
Property Detail¶
InterpolationMethod¶
-
FieldEvaluator.
InterpolationMethod
¶ Returns or sets the interpolation method used when this table data is evaluated.
-------------------------------------
Getter Method
Signature
InterpolationMethod()
Returns: the interpolation method Return type: NXOpen.Fields.FieldEvaluatorInterpolationEnum
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterpolationMethod(interpolationMethod)
Parameters: interpolationMethod ( NXOpen.Fields.FieldEvaluatorInterpolationEnum
) – the interpolation methodNew in version NX7.5.2.
License requirements: None.
Method Detail¶
Delete¶
-
FieldEvaluator.
Delete
¶ Delete this field evaluator; destroys the field evaluator and removes all references to it.
Signature
Delete()
New in version NX7.5.2.
License requirements: None.
Evaluate¶
-
FieldEvaluator.
Evaluate
¶ Evaluate the Field at the specified independent variable
NXOpen.Fields.FieldVariable
values and return the values for the specified dependent variable.The number of output values will be the same as number of independent variables specified and these values will be in the same units as the dependent variable
NXOpen.Fields.FieldVariable
.Signature
Evaluate(dependentVariable)
Parameters: dependentVariable ( NXOpen.Fields.FieldVariable
) – dependent variable whose values are to be evaluatedReturns: the values evaluated for this dependent variable Return type: list of float New in version NX7.5.2.
License requirements: None.
GetDependentVariables¶
-
FieldEvaluator.
GetDependentVariables
¶ Returns the dependent variables for this
NXOpen.Fields.FieldEvaluator
Signature
GetDependentVariables()
Returns: dependent variables for this NXOpen.Fields.FieldEvaluator
Return type: list of NXOpen.Fields.FieldVariable
New in version NX7.5.2.
License requirements: None.
GetIndependentVariables¶
-
FieldEvaluator.
GetIndependentVariables
¶ Returns the independent variables for this
NXOpen.Fields.FieldEvaluator
Signature
GetIndependentVariables()
Returns: independent variables for this NXOpen.Fields.FieldEvaluator
Return type: list of NXOpen.Fields.FieldVariable
New in version NX7.5.2.
License requirements: None.
SetIndependentVariableValues¶
-
FieldEvaluator.
SetIndependentVariableValues
¶ Sets values at which the Field will be evaluated for this independent variable
NXOpen.Fields.FieldVariable
.The number of input values mush be the same for independent variables and these values are assumed to be in the same units as the independent variable
NXOpen.Fields.FieldVariable
.Signature
SetIndependentVariableValues(independentVariable, values)
Parameters: - independentVariable (
NXOpen.Fields.FieldVariable
) – independent variable whose values are being set. - values (list of float) – the values for this independent variable where the field will be evaluated at.
New in version NX7.5.2.
License requirements: None.
- independentVariable (