UserDefinedFeatureUpdateEvent Class¶
-
class
NXOpen.Features.
UserDefinedFeatureUpdateEvent
¶ Bases:
NXOpen.TaggedObject
JA interface for the UserDefinedFeatureUpdateEvent object
This calls cannot be created
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ApplicationData | Returns the application data |
ClassName | Returns the class name |
ComponentFeature | Returns the component feature being updated |
Instantiation | Returns the UDF instantiation |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetComponentFeatures | The component features that have been updated so far @return |
GetExpressionData | The expressions of the instantiation feature @return |
GetReferenceData | The references of the instantiation feature @return |
Property Detail¶
ApplicationData¶
-
UserDefinedFeatureUpdateEvent.
ApplicationData
¶ Returns the application data
-------------------------------------
Getter Method
Signature
ApplicationData()
Returns: the application data Return type: NXOpen.Features.UserDefinedFeatureApplicationData
New in version NX8.0.0.
License requirements: None.
ClassName¶
-
UserDefinedFeatureUpdateEvent.
ClassName
¶ Returns the class name
-------------------------------------
Getter Method
Signature
ClassName()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
ComponentFeature¶
-
UserDefinedFeatureUpdateEvent.
ComponentFeature
¶ Returns the component feature being updated
-------------------------------------
Getter Method
Signature
ComponentFeature()
Returns: The feature being updated Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.
Instantiation¶
-
UserDefinedFeatureUpdateEvent.
Instantiation
¶ Returns the UDF instantiation
-------------------------------------
Getter Method
Signature
Instantiation()
Returns: The UDF instantiation that is being created Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.
Method Detail¶
GetComponentFeatures¶
-
UserDefinedFeatureUpdateEvent.
GetComponentFeatures
¶ The component features that have been updated so far
Signature
GetComponentFeatures()
Returns: Return type: list of NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.
GetExpressionData¶
-
UserDefinedFeatureUpdateEvent.
GetExpressionData
¶ The expressions of the instantiation feature
Signature
GetExpressionData()
Returns: Return type: list of NXOpen.Features.UserDefinedFeatureExpressionData
New in version NX8.0.0.
License requirements: None.
GetReferenceData¶
-
UserDefinedFeatureUpdateEvent.
GetReferenceData
¶ The references of the instantiation feature
Signature
GetReferenceData()
Returns: Return type: list of NXOpen.Features.UserDefinedFeatureReferenceData
New in version NX8.0.0.
License requirements: None.