UserDefinedFeatureApplicationData Class¶
-
class
NXOpen.Features.
UserDefinedFeatureApplicationData
¶ Bases:
NXOpen.TaggedObject
JA interface for UserDefinedFeatureApplicationData object
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
AddField | Adds named field. |
GetField | Gets named field. |
GetFields | Gets all of the fields @return Array of fields |
RemoveField | Removes named field. |
Method Detail¶
AddField¶
-
UserDefinedFeatureApplicationData.
AddField
¶ Adds named field.
Returns existing field if one exists.
Signature
AddField(name)
Parameters: name (str) – name of the field NOTE: The full Unicode character set is not supported for this parameter. Returns: the field Return type: NXOpen.Features.UserDefinedFeatureApplicationField
New in version NX8.0.0.
License requirements: None.
GetField¶
-
UserDefinedFeatureApplicationData.
GetField
¶ Gets named field.
Creates field if it doesnt exist.
Signature
GetField(name)
Parameters: name (str) – name of the field NOTE: The full Unicode character set is not supported for this parameter. Returns: the field Return type: NXOpen.Features.UserDefinedFeatureApplicationField
New in version NX8.0.0.
License requirements: None.
GetFields¶
-
UserDefinedFeatureApplicationData.
GetFields
¶ Gets all of the fields
Signature
GetFields()
Returns: Array of fields Return type: list of NXOpen.Features.UserDefinedFeatureApplicationField
New in version NX8.0.0.
License requirements: None.
RemoveField¶
-
UserDefinedFeatureApplicationData.
RemoveField
¶ Removes named field.
This removes the field and deletes it.
Signature
RemoveField(field)
Parameters: field ( NXOpen.Features.UserDefinedFeatureApplicationField
) – the fieldNew in version NX8.0.0.
License requirements: None.