UserDefinedFeatureApplicationField Class¶
-
class
NXOpen.Features.
UserDefinedFeatureApplicationField
¶ Bases:
NXOpen.TaggedObject
JA interface for UserDefinedFeatureApplicationField object
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns the name of this field |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetDoubles | Gets all of the doubles in this field @return Array of doubles in this field |
GetIntegers | Gets all of the integers stored in this field @return Array of integers in this field |
GetObjects | Gets all of the objects in this field @return Array of objects in this field |
GetStrings | Gets all of the strings in this field @return Array of strings in this field |
SetDoubles | Sets all of the doubles in this field |
SetIntegers | Sets all of the integers stored in this field |
SetObjects | Sets all of the objects in this field |
SetStrings | Sets all of the strings in this field |
Property Detail¶
Method Detail¶
GetDoubles¶
-
UserDefinedFeatureApplicationField.
GetDoubles
¶ Gets all of the doubles in this field
Signature
GetDoubles()
Returns: Array of doubles in this field Return type: list of float New in version NX8.0.0.
License requirements: None.
GetIntegers¶
-
UserDefinedFeatureApplicationField.
GetIntegers
¶ Gets all of the integers stored in this field
Signature
GetIntegers()
Returns: Array of integers in this field Return type: list of int New in version NX8.0.0.
License requirements: None.
GetObjects¶
-
UserDefinedFeatureApplicationField.
GetObjects
¶ Gets all of the objects in this field
Signature
GetObjects()
Returns: Array of objects in this field Return type: list of NXOpen.TaggedObject
New in version NX8.0.0.
License requirements: None.
GetStrings¶
-
UserDefinedFeatureApplicationField.
GetStrings
¶ Gets all of the strings in this field
Signature
GetStrings()
Returns: Array of strings in this field Return type: list of str New in version NX8.0.0.
License requirements: None.
SetDoubles¶
-
UserDefinedFeatureApplicationField.
SetDoubles
¶ Sets all of the doubles in this field
Signature
SetDoubles(doubles)
Parameters: doubles (list of float) – New Array of doubles in this field New in version NX8.0.0.
License requirements: None.
SetIntegers¶
-
UserDefinedFeatureApplicationField.
SetIntegers
¶ Sets all of the integers stored in this field
Signature
SetIntegers(integers)
Parameters: integers (list of int) – New Array of integers in this field New in version NX8.0.0.
License requirements: None.
SetObjects¶
-
UserDefinedFeatureApplicationField.
SetObjects
¶ Sets all of the objects in this field
Signature
SetObjects(objects)
Parameters: objects (list of NXOpen.TaggedObject
) – New Array of strings in this fieldNew in version NX8.0.0.
License requirements: None.
SetStrings¶
-
UserDefinedFeatureApplicationField.
SetStrings
¶ Sets all of the strings in this field
Signature
SetStrings(strings)
Parameters: strings (list of str) – New Array of strings in this field NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.0.
License requirements: None.