UserDefinedFeatureReferenceData Class¶
-
class
NXOpen.Features.
UserDefinedFeatureReferenceData
¶ Bases:
NXOpen.TaggedObject
JA interface for UserDefinedFeatureReference object.
Objects of this class contain an external reference of the user defined feature and the corresponding prompt. This cannot be created
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Prompt | Returns the prompt for this reference |
Reference | Returns the reference of a user defined feature |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
Prompt¶
-
UserDefinedFeatureReferenceData.
Prompt
¶ Returns the prompt for this reference
-------------------------------------
Getter Method
Signature
Prompt()
Returns: the prompt for this reference Return type: str New in version NX8.0.0.
License requirements: None.
Reference¶
-
UserDefinedFeatureReferenceData.
Reference
¶ Returns the reference of a user defined feature
-------------------------------------
Getter Method
Signature
Reference()
Returns: the reference of a user defined feature Return type: NXOpen.TaggedObject
New in version NX8.0.0.
License requirements: None.