SweepAlongGuideBuilder Class¶
-
class
NXOpen.Features.
SweepAlongGuideBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SweepAlongGuide
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSweepAlongGuideBuilder
Default values.
Property Value FirstOffset.Value 0.0 (millimeters part), 0.0 (inches part) SecondOffset.Value 0.0 (millimeters part), 0.0 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BooleanOperation | Returns the boolean operation |
ChainingTolerance | Returns or sets the chaining tolerance |
DistanceTolerance | Returns or sets the distance tolerance |
FeatureOptions | Returns the feature options |
FirstOffset | Returns the first offset |
Guide | Returns the guide |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SecondOffset | Returns the second offset |
Section | Returns the section |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BooleanOperation¶
-
SweepAlongGuideBuilder.
BooleanOperation
¶ Returns the boolean operation
-------------------------------------
Getter Method
Signature
BooleanOperation()
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX6.0.0.
License requirements: None.
ChainingTolerance¶
-
SweepAlongGuideBuilder.
ChainingTolerance
¶ Returns or sets the chaining tolerance
-------------------------------------
Getter Method
Signature
ChainingTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChainingTolerance(chainingTolerance)
Parameters: chainingTolerance (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTolerance¶
-
SweepAlongGuideBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FeatureOptions¶
-
SweepAlongGuideBuilder.
FeatureOptions
¶ Returns the feature options
-------------------------------------
Getter Method
Signature
FeatureOptions()
Returns: The Sweep Along Guide Feature Options Return type: NXOpen.GeometricUtilities.FeatureOptions
New in version NX6.0.0.
License requirements: None.
FirstOffset¶
-
SweepAlongGuideBuilder.
FirstOffset
¶ Returns the first offset
-------------------------------------
Getter Method
Signature
FirstOffset()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Guide¶
-
SweepAlongGuideBuilder.
Guide
¶ Returns the guide
-------------------------------------
Getter Method
Signature
Guide()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
SecondOffset¶
-
SweepAlongGuideBuilder.
SecondOffset
¶ Returns the second offset
-------------------------------------
Getter Method
Signature
SecondOffset()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Section¶
-
SweepAlongGuideBuilder.
Section
¶ Returns the section
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SweepAlongGuideBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.