FeatureOptions Class¶
-
class
NXOpen.GeometricUtilities.
FeatureOptions
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents various options supported on features.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BodyType | Returns or sets the body type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FeatureOptionsBodyStyle Enumeration | This enum represents the various body types |
Property Detail¶
BodyType¶
-
FeatureOptions.
BodyType
¶ Returns or sets the body type
-------------------------------------
Getter Method
Signature
BodyType()
Returns: body type Return type: NXOpen.GeometricUtilities.FeatureOptionsBodyStyle
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BodyType(type)
Parameters: type ( NXOpen.GeometricUtilities.FeatureOptionsBodyStyle
) – body typeNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
FeatureOptions.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.