IntersectionCurveBuilder Class¶
-
class
NXOpen.Features.
IntersectionCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.IntersectionCurveBuilder
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateIntersectionCurveBuilder
Default values.
Property Value Associative True CurveFitData.CurveJoinMethod No CurveFitData.Degree 7 CurveFitData.FitMethod DegreeAndSegments CurveFitData.IsAdvancedFit 0 CurveFitData.IsAlignShape 0 CurveFitData.MaximumDegree 7 CurveFitData.MaximumSegments 1 CurveFitData.MinimumDegree 5 CurveFitData.Segments 1 CurveFitOptions.FitOption Cubic CurveFitOptions.MaximumDegree 7 CurveFitOptions.MaximumSegments 1 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
CurveFitData | Returns the curve fit settings |
CurveFitOptions | Returns the curve fit options |
FirstFace | Returns the first face |
FirstPlane | Returns or sets the first plane |
FirstSet | Returns the first set required only for non-associative intersection curve |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SecondFace | Returns the second face |
SecondPlane | Returns or sets the second plane |
SecondSet | Returns the second set required only for non-associative intersection curve |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Associative¶
-
IntersectionCurveBuilder.
Associative
¶ Returns or sets the associative
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CurveFitData¶
-
IntersectionCurveBuilder.
CurveFitData
¶ Returns the curve fit settings
-------------------------------------
Getter Method
Signature
CurveFitData()
Returns: Return type: NXOpen.GeometricUtilities.CurveFitData
New in version NX8.0.0.
License requirements: None.
CurveFitOptions¶
-
IntersectionCurveBuilder.
CurveFitOptions
¶ Returns the curve fit options
-------------------------------------
Getter Method
Signature
CurveFitOptions()
Returns: curve fit options Return type: NXOpen.GeometricUtilities.CurveFitOptions
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FirstFace¶
-
IntersectionCurveBuilder.
FirstFace
¶ Returns the first face
-------------------------------------
Getter Method
Signature
FirstFace()
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
FirstPlane¶
-
IntersectionCurveBuilder.
FirstPlane
¶ Returns or sets the first plane
-------------------------------------
Getter Method
Signature
FirstPlane()
Returns: Return type: NXOpen.Plane
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstPlane(firstPlane)
Parameters: firstPlane ( NXOpen.Plane
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FirstSet¶
-
IntersectionCurveBuilder.
FirstSet
¶ Returns the first set required only for non-associative intersection curve
-------------------------------------
Getter Method
Signature
FirstSet()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
SecondFace¶
-
IntersectionCurveBuilder.
SecondFace
¶ Returns the second face
-------------------------------------
Getter Method
Signature
SecondFace()
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
SecondPlane¶
-
IntersectionCurveBuilder.
SecondPlane
¶ Returns or sets the second plane
-------------------------------------
Getter Method
Signature
SecondPlane()
Returns: Return type: NXOpen.Plane
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondPlane(secondPlane)
Parameters: secondPlane ( NXOpen.Plane
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondSet¶
-
IntersectionCurveBuilder.
SecondSet
¶ Returns the second set required only for non-associative intersection curve
-------------------------------------
Getter Method
Signature
SecondSet()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
Tolerance¶
-
IntersectionCurveBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
IntersectionCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.