EditDimensionBuilder Class¶
-
class
NXOpen.Features.
EditDimensionBuilder
¶ Bases:
NXOpen.Builder
Represents a builder of edit feature dimensions
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateEditDimensionBuilder
Default values.
Property Value DisplayAsPmi 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Dimension | Returns the feature dimension |
DisplayAsPmi | Returns or sets the display as pmi flag |
FeatureSet | Returns the list of features |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AttachToNewGeometry | Attach the given dimension to new geometry |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Dimension¶
-
EditDimensionBuilder.
Dimension
¶ Returns the feature dimension
-------------------------------------
Getter Method
Signature
Dimension()
Returns: Return type: NXOpen.Annotations.SelectAnnotation
New in version NX6.0.0.
License requirements: None.
DisplayAsPmi¶
-
EditDimensionBuilder.
DisplayAsPmi
¶ Returns or sets the display as pmi flag
-------------------------------------
Getter Method
Signature
DisplayAsPmi()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayAsPmi(displayAsPmi)
Parameters: displayAsPmi (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FeatureSet¶
-
EditDimensionBuilder.
FeatureSet
¶ Returns the list of features
-------------------------------------
Getter Method
Signature
FeatureSet()
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
AttachToNewGeometry¶
-
EditDimensionBuilder.
AttachToNewGeometry
¶ Attach the given dimension to new geometry
Signature
AttachToNewGeometry(dimTag, newGeometry)
Parameters: - dimTag (
NXOpen.Annotations.Annotation
) – - newGeometry (
NXOpen.DisplayableObject
) –
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- dimTag (
Validate¶
-
EditDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.