DividefaceBuilder Class¶
-
class
NXOpen.Features.
DividefaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a divide face builder
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateDividefaceBuilder
Default values.
Property Value SelectDividingObject.OffsetDistance.Value 5 (millimeters part), 0.2 (inches part) SelectDividingObject.ToolOption Object New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BlankOption | Returns or sets the curve blanking option |
DividingObjectsList | Returns the Dividing Objects |
ExtendOption | Returns or sets the Extend resulting edges to boundary |
FacesToDivide | Returns or sets the Faces to Divide |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProjectCurvesThatLieOnFaceOption | Returns or sets the Do not project curves that lie on face |
ProjectionOption | Returns the Projection Options data |
SelectDividingObject | Returns the Select Dividing Objects |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BlankOption¶
-
DividefaceBuilder.
BlankOption
¶ Returns or sets the curve blanking option
-------------------------------------
Getter Method
Signature
BlankOption()
Returns: false: maintain curves; true: blank curves Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankOption(blank)
Parameters: blank (bool) – false: maintain curves; true: blank curves New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
DividingObjectsList¶
-
DividefaceBuilder.
DividingObjectsList
¶ Returns the Dividing Objects
-------------------------------------
Getter Method
Signature
DividingObjectsList()
Returns: dividing objects list. List contains Section and ScCollector Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.0.
Deprecated since version NX9.0.0: This is for pre NX9 usage, do not use this method. Instead use
NXOpen.Features.DividefaceBuilder.SelectDividingObject
instead.License requirements: None.
ExtendOption¶
-
DividefaceBuilder.
ExtendOption
¶ Returns or sets the Extend resulting edges to boundary
-------------------------------------
Getter Method
Signature
ExtendOption()
Returns: false: do not extend curves; true: extend curves Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendOption(extend)
Parameters: extend (bool) – false: do not extend curves; true: extend curves New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
FacesToDivide¶
-
DividefaceBuilder.
FacesToDivide
¶ Returns or sets the Faces to Divide
-------------------------------------
Getter Method
Signature
FacesToDivide()
Returns: Smart collector for faces to divide Return type: NXOpen.ScCollector
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FacesToDivide(facesToDivide)
Parameters: facesToDivide ( NXOpen.ScCollector
) – Smart collector for faces to divideNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
ProjectCurvesThatLieOnFaceOption¶
-
DividefaceBuilder.
ProjectCurvesThatLieOnFaceOption
¶ Returns or sets the Do not project curves that lie on face
-------------------------------------
Getter Method
Signature
ProjectCurvesThatLieOnFaceOption()
Returns: false: project curves that lie on face option; true: Do not project curves that lie on face option Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectCurvesThatLieOnFaceOption(projectCurvesThatLieOnFace)
Parameters: projectCurvesThatLieOnFace (bool) – false: project curves that lie on face option; true: Do not project curves that lie on face option New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
ProjectionOption¶
-
DividefaceBuilder.
ProjectionOption
¶ Returns the Projection Options data
-------------------------------------
Getter Method
Signature
ProjectionOption()
Returns: Projection Options data Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX4.0.0.
License requirements: None.
SelectDividingObject¶
-
DividefaceBuilder.
SelectDividingObject
¶ Returns the Select Dividing Objects
-------------------------------------
Getter Method
Signature
SelectDividingObject()
Returns: dividing objects Return type: NXOpen.GeometricUtilities.SelectDividingObjectBuilder
New in version NX9.0.0.
License requirements: None.
Tolerance¶
-
DividefaceBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Tolerance Return type: float New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – Tolerance New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
DividefaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.