DeleteFaceBuilder Class¶
-
class
NXOpen.Features.
DeleteFaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder for a delete face feature, don’t use it until nx502.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateDeleteFaceBuilder
Default values.
Property Value CapOption FaceOrPlane DeletePartialBlend False FaceEdgeBlendPreference Cliff Heal True HealPlanar False MaxBlendRadius.Value 5.0 (millimeters part), 0.2 (inches part) MaxHoleDiameter.Value 5.0 (millimeters part), 0.2 (inches part) Setback SelectedBlend SpecifyBlend False UseHoleDiameter True New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
BlendCollector | Returns the blend collector holding the blends to delete |
CapFace | Returns the face or plane to be used as cap face. |
CapOption | Returns or sets the cap option. |
CapPlane | Returns or sets the new plane to be used as cap face. |
DeletePartialBlend | Returns or sets the flag indicating whether to delete the partial blend or not. |
FaceCollector | Returns the face collector holding the faces to delete, don’t use it until nx502 |
FaceEdgeBlendPreference | Returns or sets the preference option indicating wether to delete undetermined blend chain as notch chain or as cliff chain |
Heal | Returns or sets the flag specifying whether to heal the body while deleting its face. |
HealPlanar | Returns or sets the flag of finding a plane in which all edges of a hole lie and attach this to a face covering the hole during heal hole process, don’t use it until further notification |
MaxBlendRadius | Returns the maximal radius of deleted blends, only for delete blend type |
MaxHoleDiameter | Returns the maximal diameter of deleted holes, only for delete hole type and only working when use_hole_diameter is true, don’t use it until nx502 |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Setback | Returns or sets the set back options. |
SpecifyBlend | Returns or sets the flag of treating all input faces as blend, don’t use it until further notification |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the delete face type, don’t use it until nx502 |
UseHoleDiameter | Returns or sets the flag of using hole diameter to filter hole or not, only for delete hole type and the max hole diameter should be set if it is true, don’t use it until nx502 |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DeleteFaceBuilderCapOptionValues Enumeration | Represents the cap option values. |
DeleteFaceBuilderFaceEdgeBlendPreferenceOptions Enumeration | Represents the face edge blend preference options. |
DeleteFaceBuilderSelectTypes Enumeration | Enumeration of select type, don’t use it until nx502 |
DeleteFaceBuilderSetbackOptions Enumeration | Represents the set back options. |
Property Detail¶
BlendCollector¶
-
DeleteFaceBuilder.
BlendCollector
¶ Returns the blend collector holding the blends to delete
-------------------------------------
Getter Method
Signature
BlendCollector()
Returns: the delete blend collector Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
CapFace¶
-
DeleteFaceBuilder.
CapFace
¶ Returns the face or plane to be used as cap face.
-------------------------------------
Getter Method
Signature
CapFace()
Returns: Return type: NXOpen.SelectISurface
New in version NX8.0.1.
License requirements: None.
CapOption¶
-
DeleteFaceBuilder.
CapOption
¶ Returns or sets the cap option.
-------------------------------------
Getter Method
Signature
CapOption()
Returns: Return type: NXOpen.Features.DeleteFaceBuilderCapOptionValues
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CapOption(capOption)
Parameters: capOption ( NXOpen.Features.DeleteFaceBuilderCapOptionValues
) –New in version NX8.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
CapPlane¶
-
DeleteFaceBuilder.
CapPlane
¶ Returns or sets the new plane to be used as cap face.
-------------------------------------
Getter Method
Signature
CapPlane()
Returns: Return type: NXOpen.Plane
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CapPlane(capPlane)
Parameters: capPlane ( NXOpen.Plane
) –New in version NX8.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
DeletePartialBlend¶
-
DeleteFaceBuilder.
DeletePartialBlend
¶ Returns or sets the flag indicating whether to delete the partial blend or not.
-------------------------------------
Getter Method
Signature
DeletePartialBlend()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeletePartialBlend(deletePartialBlend)
Parameters: deletePartialBlend (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
FaceCollector¶
-
DeleteFaceBuilder.
FaceCollector
¶ Returns the face collector holding the faces to delete, don’t use it until nx502
-------------------------------------
Getter Method
Signature
FaceCollector()
Returns: the delete face collector Return type: NXOpen.ScCollector
New in version NX5.0.2.
License requirements: None.
FaceEdgeBlendPreference¶
-
DeleteFaceBuilder.
FaceEdgeBlendPreference
¶ Returns or sets the preference option indicating wether to delete undetermined blend chain as notch chain or as cliff chain
-------------------------------------
Getter Method
Signature
FaceEdgeBlendPreference()
Returns: Return type: NXOpen.Features.DeleteFaceBuilderFaceEdgeBlendPreferenceOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceEdgeBlendPreference(faceEdgeBlendPreference)
Parameters: faceEdgeBlendPreference ( NXOpen.Features.DeleteFaceBuilderFaceEdgeBlendPreferenceOptions
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Heal¶
-
DeleteFaceBuilder.
Heal
¶ Returns or sets the flag specifying whether to heal the body while deleting its face.
If True, body is healed, else it is not.
-------------------------------------
Getter Method
Signature
Heal()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Heal(heal)
Parameters: heal (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
HealPlanar¶
-
DeleteFaceBuilder.
HealPlanar
¶ Returns or sets the flag of finding a plane in which all edges of a hole lie and attach this to a face covering the hole during heal hole process, don’t use it until further notification
-------------------------------------
Getter Method
Signature
HealPlanar()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HealPlanar(healPlanar)
Parameters: healPlanar (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
MaxBlendRadius¶
-
DeleteFaceBuilder.
MaxBlendRadius
¶ Returns the maximal radius of deleted blends, only for delete blend type
-------------------------------------
Getter Method
Signature
MaxBlendRadius()
Returns: the maximal radius expression Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
MaxHoleDiameter¶
-
DeleteFaceBuilder.
MaxHoleDiameter
¶ Returns the maximal diameter of deleted holes, only for delete hole type and only working when use_hole_diameter is true, don’t use it until nx502
-------------------------------------
Getter Method
Signature
MaxHoleDiameter()
Returns: the maximal diameter expression Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
Setback¶
-
DeleteFaceBuilder.
Setback
¶ Returns or sets the set back options.
-------------------------------------
Getter Method
Signature
Setback()
Returns: Return type: NXOpen.Features.DeleteFaceBuilderSetbackOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Setback(setback)
Parameters: setback ( NXOpen.Features.DeleteFaceBuilderSetbackOptions
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
SpecifyBlend¶
-
DeleteFaceBuilder.
SpecifyBlend
¶ Returns or sets the flag of treating all input faces as blend, don’t use it until further notification
-------------------------------------
Getter Method
Signature
SpecifyBlend()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecifyBlend(specifyBlend)
Parameters: specifyBlend (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Type¶
-
DeleteFaceBuilder.
Type
¶ Returns or sets the delete face type, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Type()
Returns: the delete face type Return type: NXOpen.Features.DeleteFaceBuilderSelectTypes
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(selectType)
Parameters: selectType ( NXOpen.Features.DeleteFaceBuilderSelectTypes
) – the delete face typeNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
UseHoleDiameter¶
-
DeleteFaceBuilder.
UseHoleDiameter
¶ Returns or sets the flag of using hole diameter to filter hole or not, only for delete hole type and the max hole diameter should be set if it is true, don’t use it until nx502
-------------------------------------
Getter Method
Signature
UseHoleDiameter()
Returns: the flag of use hole diameter Return type: bool New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseHoleDiameter(useHoleDiameter)
Parameters: useHoleDiameter (bool) – the flag of use hole diameter New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
DeleteFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.