CurveLengthBuilder Class¶
-
class
NXOpen.Features.
CurveLengthBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents the CurveLength builder
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateCurvelengthBuilder
Default values.
Property Value CurveOptions.Associative True New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
CurveOptions | Returns the CurveOptions |
CurvelengthData | Returns the curvelength data |
DistanceTolerance | Returns or sets the distance tolerance |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Section | Returns or sets the section |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CurveOptions¶
-
CurveLengthBuilder.
CurveOptions
¶ Returns the CurveOptions
-------------------------------------
Getter Method
Signature
CurveOptions()
Returns: Curve Options Return type: NXOpen.GeometricUtilities.CurveOptions
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CurvelengthData¶
-
CurveLengthBuilder.
CurvelengthData
¶ Returns the curvelength data
-------------------------------------
Getter Method
Signature
CurvelengthData()
Returns: CurveLength data Return type: NXOpen.GeometricUtilities.CurveLengthData
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTolerance¶
-
CurveLengthBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: CurveLength chaining tolerance Return type: float New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – CurveLength chaining tolerance New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Section¶
-
CurveLengthBuilder.
Section
¶ Returns or sets the section
-------------------------------------
Getter Method
Signature
Section()
Returns: Section object Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
Section(section)
Parameters: section ( NXOpen.Section
) – Section object This parameter may not be None.New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
CurveLengthBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.