BridgeCurveBuilder Class¶
-
class
NXOpen.Features.
BridgeCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.BridgeCurve
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateBridgeCurveBuilder
Default values.
Property Value CurveFitData.CurveJoinMethod No CurveFitData.Degree 7 CurveFitData.FitMethod DegreeAndSegments CurveFitData.IsAdvancedFit 0 CurveFitData.IsAlignShape 0 CurveFitData.MaximumDegree 7 CurveFitData.MaximumSegments 1 CurveFitData.MinimumDegree 5 CurveFitData.Segments 1 Depth.Value 50 EndDirectionAngle.Value 0 EndTangentMagnitude.Value 1 IsAssociative True MinimumRadiusValue.Value 1 ReverseEndDirection False ReverseStartDirection False Rho.Value 0.5 Skew.Value 50 StartDirectionAngle.Value 0 StartTangentMagnitude.Value 1 UPercentEnd.Value 0 UPercentStart.Value 0 VPercentEnd.Value 0 VPercentStart.Value 0 New in version NX5.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Features.BridgeCurveBuilderEx
instead.
Properties¶
Property | Description |
---|---|
ConstraintFaces | Returns the constraint faces |
CurveFitData | Returns the curve fitting parameters |
CurveFitOption | Returns or sets the curve fit option |
Depth | Returns the depth value for shape control option of NXOpen.Features.BridgeCurveBuilderShapeControlTypes.PeakPoint |
EndContinuityOption | Returns or sets the end continuity option |
EndCurveDirectionOption | Returns or sets the end curve direction option |
EndDirectionAngle | Returns the end direction angle |
EndObject | Returns the end object |
EndObjectOption | Returns or sets the object selection option |
EndPerpendicularFace | Returns the end perpendicular face |
EndPointDirection | Returns or sets the end point direction |
EndReferencePoint | Returns or sets the start reference point |
EndSurfaceDirectionOption | Returns or sets the end surface direction option |
EndTangentMagnitude | Returns the end tangent magnitude for shape control option of NXOpen.Features.BridgeCurveBuilderShapeControlTypes.EndPoint |
EndVectorObject | Returns or sets the start point direction |
IsAssociative | Returns or sets whether the bridge curve is associative |
MaximumDegree | Returns or sets the maximum degree |
MaximumSegment | Returns or sets the maximum segment |
MinimumRadiusOption | Returns or sets the minimum radius option |
MinimumRadiusValue | Returns the minimum radius value |
ObjectSelectionOption | Returns or sets the object selection option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseEndDirection | Returns or sets the reverse end direction |
ReverseStartDirection | Returns or sets the reverse start direction |
Rho | Returns the rho value for shape control option of NXOpen.Features.BridgeCurveBuilderShapeControlTypes.Conic |
ShapeControlOption | Returns or sets the shape control option |
ShapeCurve | Returns the shape curve for shape control option of NXOpen.Features.BridgeCurveBuilderShapeControlTypes.ShapeCurve |
Skew | Returns the skew value for shape control option of NXOpen.Features.BridgeCurveBuilderShapeControlTypes.PeakPoint |
StartContinuityOption | Returns or sets the start continuity option |
StartCurveDirectionOption | Returns or sets the start curve direction option |
StartDirectionAngle | Returns the start direction angle |
StartObject | Returns the start object |
StartPerpendicularFace | Returns the start perpendicular face |
StartPointDirection | Returns or sets the start point direction |
StartReferencePoint | Returns or sets the start reference point |
StartSurfaceDirectionOption | Returns or sets the start surface direction option |
StartTangentMagnitude | Returns the start tangent magnitude for shape control option of NXOpen.Features.BridgeCurveBuilderShapeControlTypes.EndPoint |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
UPercentEnd | Returns the u percent end |
UPercentStart | Returns the u percent start |
VPercentEnd | Returns the v percent end |
VPercentStart | Returns the v percent start |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BridgeCurveBuilderConstraintTypes Enumeration | This enum represents the end continuity constraint types for the bridge curve |
BridgeCurveBuilderCurveDirectionTypes Enumeration | This enum represents the direction type for input curves |
BridgeCurveBuilderCurveFitTypes Enumeration | This enum represents the curve fit types for the bridge curve |
BridgeCurveBuilderEndObjectTypes Enumeration | This enum represents the current selected end object types for the bridge curve |
BridgeCurveBuilderMinRadiusTypes Enumeration | This enum represents the minimum radius types for the bridge curve |
BridgeCurveBuilderSelectedObject Enumeration | This enum represents the current selected object for the bridge curve |
BridgeCurveBuilderShapeControlTypes Enumeration | This enum represents the shape control types for the bridge curve |
BridgeCurveBuilderSurfaceDirectionTypes Enumeration | This enum represents the direction type for input surfaces |
Property Detail¶
ConstraintFaces¶
-
BridgeCurveBuilder.
ConstraintFaces
¶ Returns the constraint faces
-------------------------------------
Getter Method
Signature
ConstraintFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
CurveFitData¶
-
BridgeCurveBuilder.
CurveFitData
¶ Returns the curve fitting parameters
-------------------------------------
Getter Method
Signature
CurveFitData()
Returns: Return type: NXOpen.GeometricUtilities.CurveFitData
New in version NX8.5.0.
License requirements: None.
CurveFitOption¶
-
BridgeCurveBuilder.
CurveFitOption
¶ Returns or sets the curve fit option
-------------------------------------
Getter Method
Signature
CurveFitOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderCurveFitTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveFitOption(curveFitOption)
Parameters: curveFitOption ( NXOpen.Features.BridgeCurveBuilderCurveFitTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
Depth¶
-
BridgeCurveBuilder.
Depth
¶ Returns the depth value for shape control option of
NXOpen.Features.BridgeCurveBuilderShapeControlTypes.PeakPoint
-------------------------------------
Getter Method
Signature
Depth()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
EndContinuityOption¶
-
BridgeCurveBuilder.
EndContinuityOption
¶ Returns or sets the end continuity option
-------------------------------------
Getter Method
Signature
EndContinuityOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderConstraintTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndContinuityOption(endContinuityOption)
Parameters: endContinuityOption ( NXOpen.Features.BridgeCurveBuilderConstraintTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
EndCurveDirectionOption¶
-
BridgeCurveBuilder.
EndCurveDirectionOption
¶ Returns or sets the end curve direction option
-------------------------------------
Getter Method
Signature
EndCurveDirectionOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderCurveDirectionTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCurveDirectionOption(endCurveDirectionOption)
Parameters: endCurveDirectionOption ( NXOpen.Features.BridgeCurveBuilderCurveDirectionTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
EndDirectionAngle¶
-
BridgeCurveBuilder.
EndDirectionAngle
¶ Returns the end direction angle
-------------------------------------
Getter Method
Signature
EndDirectionAngle()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
EndObject¶
-
BridgeCurveBuilder.
EndObject
¶ Returns the end object
-------------------------------------
Getter Method
Signature
EndObject()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
EndObjectOption¶
-
BridgeCurveBuilder.
EndObjectOption
¶ Returns or sets the object selection option
-------------------------------------
Getter Method
Signature
EndObjectOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderEndObjectTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndObjectOption(endObjectOption)
Parameters: endObjectOption ( NXOpen.Features.BridgeCurveBuilderEndObjectTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
EndPerpendicularFace¶
-
BridgeCurveBuilder.
EndPerpendicularFace
¶ Returns the end perpendicular face
-------------------------------------
Getter Method
Signature
EndPerpendicularFace()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
EndPointDirection¶
-
BridgeCurveBuilder.
EndPointDirection
¶ Returns or sets the end point direction
-------------------------------------
Getter Method
Signature
EndPointDirection()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPointDirection(endPointDirection)
Parameters: endPointDirection ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
EndReferencePoint¶
-
BridgeCurveBuilder.
EndReferencePoint
¶ Returns or sets the start reference point
-------------------------------------
Getter Method
Signature
EndReferencePoint()
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndReferencePoint(endReferencePoint)
Parameters: endReferencePoint ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
EndSurfaceDirectionOption¶
-
BridgeCurveBuilder.
EndSurfaceDirectionOption
¶ Returns or sets the end surface direction option
-------------------------------------
Getter Method
Signature
EndSurfaceDirectionOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderSurfaceDirectionTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndSurfaceDirectionOption(endSurfaceDirectionOption)
Parameters: endSurfaceDirectionOption ( NXOpen.Features.BridgeCurveBuilderSurfaceDirectionTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
EndTangentMagnitude¶
-
BridgeCurveBuilder.
EndTangentMagnitude
¶ Returns the end tangent magnitude for shape control option of
NXOpen.Features.BridgeCurveBuilderShapeControlTypes.EndPoint
-------------------------------------
Getter Method
Signature
EndTangentMagnitude()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
EndVectorObject¶
-
BridgeCurveBuilder.
EndVectorObject
¶ Returns or sets the start point direction
-------------------------------------
Getter Method
Signature
EndVectorObject()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndVectorObject(endVectorObject)
Parameters: endVectorObject ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
IsAssociative¶
-
BridgeCurveBuilder.
IsAssociative
¶ Returns or sets whether the bridge curve is associative
-------------------------------------
Getter Method
Signature
IsAssociative()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsAssociative(associative)
Parameters: associative (bool) – New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
MaximumDegree¶
-
BridgeCurveBuilder.
MaximumDegree
¶ Returns or sets the maximum degree
-------------------------------------
Getter Method
Signature
MaximumDegree()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumDegree(maximumDegree)
Parameters: maximumDegree (int) – New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
MaximumSegment¶
-
BridgeCurveBuilder.
MaximumSegment
¶ Returns or sets the maximum segment
-------------------------------------
Getter Method
Signature
MaximumSegment()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumSegment(maximumSegment)
Parameters: maximumSegment (int) – New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
MinimumRadiusOption¶
-
BridgeCurveBuilder.
MinimumRadiusOption
¶ Returns or sets the minimum radius option
-------------------------------------
Getter Method
Signature
MinimumRadiusOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderMinRadiusTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumRadiusOption(minimumRadiusOption)
Parameters: minimumRadiusOption ( NXOpen.Features.BridgeCurveBuilderMinRadiusTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
MinimumRadiusValue¶
-
BridgeCurveBuilder.
MinimumRadiusValue
¶ Returns the minimum radius value
-------------------------------------
Getter Method
Signature
MinimumRadiusValue()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ObjectSelectionOption¶
-
BridgeCurveBuilder.
ObjectSelectionOption
¶ Returns or sets the object selection option
-------------------------------------
Getter Method
Signature
ObjectSelectionOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderSelectedObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectSelectionOption(objectSelectionOption)
Parameters: objectSelectionOption ( NXOpen.Features.BridgeCurveBuilderSelectedObject
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
ReverseEndDirection¶
-
BridgeCurveBuilder.
ReverseEndDirection
¶ Returns or sets the reverse end direction
-------------------------------------
Getter Method
Signature
ReverseEndDirection()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseEndDirection(reverseEndDirection)
Parameters: reverseEndDirection (bool) – New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
ReverseStartDirection¶
-
BridgeCurveBuilder.
ReverseStartDirection
¶ Returns or sets the reverse start direction
-------------------------------------
Getter Method
Signature
ReverseStartDirection()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseStartDirection(reverseStartDirection)
Parameters: reverseStartDirection (bool) – New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
Rho¶
-
BridgeCurveBuilder.
Rho
¶ Returns the rho value for shape control option of
NXOpen.Features.BridgeCurveBuilderShapeControlTypes.Conic
-------------------------------------
Getter Method
Signature
Rho()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ShapeControlOption¶
-
BridgeCurveBuilder.
ShapeControlOption
¶ Returns or sets the shape control option
-------------------------------------
Getter Method
Signature
ShapeControlOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderShapeControlTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShapeControlOption(shapeControlOption)
Parameters: shapeControlOption ( NXOpen.Features.BridgeCurveBuilderShapeControlTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
ShapeCurve¶
-
BridgeCurveBuilder.
ShapeCurve
¶ Returns the shape curve for shape control option of
NXOpen.Features.BridgeCurveBuilderShapeControlTypes.ShapeCurve
-------------------------------------
Getter Method
Signature
ShapeCurve()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
Skew¶
-
BridgeCurveBuilder.
Skew
¶ Returns the skew value for shape control option of
NXOpen.Features.BridgeCurveBuilderShapeControlTypes.PeakPoint
-------------------------------------
Getter Method
Signature
Skew()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
StartContinuityOption¶
-
BridgeCurveBuilder.
StartContinuityOption
¶ Returns or sets the start continuity option
-------------------------------------
Getter Method
Signature
StartContinuityOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderConstraintTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartContinuityOption(startContinuityOption)
Parameters: startContinuityOption ( NXOpen.Features.BridgeCurveBuilderConstraintTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
StartCurveDirectionOption¶
-
BridgeCurveBuilder.
StartCurveDirectionOption
¶ Returns or sets the start curve direction option
-------------------------------------
Getter Method
Signature
StartCurveDirectionOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderCurveDirectionTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartCurveDirectionOption(startCurveDirectionOption)
Parameters: startCurveDirectionOption ( NXOpen.Features.BridgeCurveBuilderCurveDirectionTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
StartDirectionAngle¶
-
BridgeCurveBuilder.
StartDirectionAngle
¶ Returns the start direction angle
-------------------------------------
Getter Method
Signature
StartDirectionAngle()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
StartObject¶
-
BridgeCurveBuilder.
StartObject
¶ Returns the start object
-------------------------------------
Getter Method
Signature
StartObject()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
StartPerpendicularFace¶
-
BridgeCurveBuilder.
StartPerpendicularFace
¶ Returns the start perpendicular face
-------------------------------------
Getter Method
Signature
StartPerpendicularFace()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
StartPointDirection¶
-
BridgeCurveBuilder.
StartPointDirection
¶ Returns or sets the start point direction
-------------------------------------
Getter Method
Signature
StartPointDirection()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPointDirection(startPointDirection)
Parameters: startPointDirection ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
StartReferencePoint¶
-
BridgeCurveBuilder.
StartReferencePoint
¶ Returns or sets the start reference point
-------------------------------------
Getter Method
Signature
StartReferencePoint()
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartReferencePoint(startReferencePoint)
Parameters: startReferencePoint ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
StartSurfaceDirectionOption¶
-
BridgeCurveBuilder.
StartSurfaceDirectionOption
¶ Returns or sets the start surface direction option
-------------------------------------
Getter Method
Signature
StartSurfaceDirectionOption()
Returns: Return type: NXOpen.Features.BridgeCurveBuilderSurfaceDirectionTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartSurfaceDirectionOption(startSurfaceDirectionOption)
Parameters: startSurfaceDirectionOption ( NXOpen.Features.BridgeCurveBuilderSurfaceDirectionTypes
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
StartTangentMagnitude¶
-
BridgeCurveBuilder.
StartTangentMagnitude
¶ Returns the start tangent magnitude for shape control option of
NXOpen.Features.BridgeCurveBuilderShapeControlTypes.EndPoint
-------------------------------------
Getter Method
Signature
StartTangentMagnitude()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Tolerance¶
-
BridgeCurveBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”), solid_modeling (“SOLIDS MODELING”)
UPercentEnd¶
-
BridgeCurveBuilder.
UPercentEnd
¶ Returns the u percent end
-------------------------------------
Getter Method
Signature
UPercentEnd()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
UPercentStart¶
-
BridgeCurveBuilder.
UPercentStart
¶ Returns the u percent start
-------------------------------------
Getter Method
Signature
UPercentStart()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
VPercentEnd¶
-
BridgeCurveBuilder.
VPercentEnd
¶ Returns the v percent end
-------------------------------------
Getter Method
Signature
VPercentEnd()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
VPercentStart¶
-
BridgeCurveBuilder.
VPercentStart
¶ Returns the v percent start
-------------------------------------
Getter Method
Signature
VPercentStart()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BridgeCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.