BridgeCurveBuilderCurveDirectionTypes Enumeration¶
NXOpen.Features.BridgeCurveBuilder.CurveDirectionTypes is an alias for NXOpen.Features.BridgeCurveBuilderCurveDirectionTypes
-
class
NXOpen.Features.
BridgeCurveBuilderCurveDirectionTypes
¶ Bases:
object
This enum represents the direction type for input curves
Enum Members
- of the base curve at the selected point “
- “Perpendicular”, ” bridge direction takes the direction that is
perpendicular to the tangent direction of the base curve at the selected point “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.