AeroRibBuilder Class¶
-
class
NXOpen.Features.
AeroRibBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.AeroRib
builderTo create a new instance of this class, use
NXOpen.Features.AeroCollection.CreateAeroRibBuilder
Default values.
Property Value GuideObjectType Face Height.Value 25 (millimeters part), 1 (inches part) HeightDimensionType Simple Limit1Offset.Value 0 (millimeters part), 0 (inches part) Limit1Type FromGuideCurve Limit2Offset.Value 0 (millimeters part), 0 (inches part) Limit2Type FromGuideCurve Thickness.Value 2 (millimeters part), 0.1 (inches part) ThicknessDimensionType Symmetric New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
GuideFaces | Returns the guide faces |
GuideObjectType | Returns or sets the guide object type |
Height | Returns the height |
HeightDimensionType | Returns or sets the height dimension type |
Limit1Offset | Returns the limit1 offset |
Limit1Selection | Returns the limit1 selection |
Limit1Type | Returns or sets the limit1 type |
Limit2Offset | Returns the limit2 offset |
Limit2Selection | Returns the limit2 selection |
Limit2Type | Returns or sets the limit2 type |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Plane | Returns or sets the plane |
ReverseHeightDirection | Returns or sets the reverse height direction flag. |
ReverseThicknessDirection | Returns or sets the reverse thickness direction flag. |
Section | Returns the section |
SkinFaceCollector | Returns the skin face collector |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Thickness | Returns the thickness |
ThicknessDimensionType | Returns or sets the thickness dimension type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AeroRibBuilderGuideObjectTypes Enumeration | This attribute represents the Guide Object types |
AeroRibBuilderHeightDimensionOptions Enumeration | This attribute represents the options for height dimension |
AeroRibBuilderLimitObjectTypes Enumeration | This attribute represents the limit object types |
AeroRibBuilderThicknessDimensionOptions Enumeration | This attribute represents the options for thickness dimension |
Property Detail¶
GuideFaces¶
-
AeroRibBuilder.
GuideFaces
¶ Returns the guide faces
-------------------------------------
Getter Method
Signature
GuideFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
GuideObjectType¶
-
AeroRibBuilder.
GuideObjectType
¶ Returns or sets the guide object type
-------------------------------------
Getter Method
Signature
GuideObjectType()
Returns: Return type: NXOpen.Features.AeroRibBuilderGuideObjectTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GuideObjectType(guideObjectType)
Parameters: guideObjectType ( NXOpen.Features.AeroRibBuilderGuideObjectTypes
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Height¶
-
AeroRibBuilder.
Height
¶ Returns the height
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
HeightDimensionType¶
-
AeroRibBuilder.
HeightDimensionType
¶ Returns or sets the height dimension type
-------------------------------------
Getter Method
Signature
HeightDimensionType()
Returns: Return type: NXOpen.Features.AeroRibBuilderHeightDimensionOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeightDimensionType(heightDimensionType)
Parameters: heightDimensionType ( NXOpen.Features.AeroRibBuilderHeightDimensionOptions
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Limit1Offset¶
-
AeroRibBuilder.
Limit1Offset
¶ Returns the limit1 offset
-------------------------------------
Getter Method
Signature
Limit1Offset()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Limit1Selection¶
-
AeroRibBuilder.
Limit1Selection
¶ Returns the limit1 selection
-------------------------------------
Getter Method
Signature
Limit1Selection()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
Limit1Type¶
-
AeroRibBuilder.
Limit1Type
¶ Returns or sets the limit1 type
-------------------------------------
Getter Method
Signature
Limit1Type()
Returns: Return type: NXOpen.Features.AeroRibBuilderLimitObjectTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Limit1Type(limit1Type)
Parameters: limit1Type ( NXOpen.Features.AeroRibBuilderLimitObjectTypes
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Limit2Offset¶
-
AeroRibBuilder.
Limit2Offset
¶ Returns the limit2 offset
-------------------------------------
Getter Method
Signature
Limit2Offset()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Limit2Selection¶
-
AeroRibBuilder.
Limit2Selection
¶ Returns the limit2 selection
-------------------------------------
Getter Method
Signature
Limit2Selection()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
Limit2Type¶
-
AeroRibBuilder.
Limit2Type
¶ Returns or sets the limit2 type
-------------------------------------
Getter Method
Signature
Limit2Type()
Returns: Return type: NXOpen.Features.AeroRibBuilderLimitObjectTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Limit2Type(limit2Type)
Parameters: limit2Type ( NXOpen.Features.AeroRibBuilderLimitObjectTypes
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Plane¶
-
AeroRibBuilder.
Plane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
Plane()
Returns: Return type: NXOpen.Plane
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane(plane)
Parameters: plane ( NXOpen.Plane
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseHeightDirection¶
-
AeroRibBuilder.
ReverseHeightDirection
¶ Returns or sets the reverse height direction flag.
Indicates whether the height direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseHeightDirection()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseHeightDirection(reverseHeightDirection)
Parameters: reverseHeightDirection (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseThicknessDirection¶
-
AeroRibBuilder.
ReverseThicknessDirection
¶ Returns or sets the reverse thickness direction flag.
Indicates whether the thickness direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseThicknessDirection()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseThicknessDirection(reverseThicknessDirection)
Parameters: reverseThicknessDirection (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Section¶
-
AeroRibBuilder.
Section
¶ Returns the section
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
SkinFaceCollector¶
-
AeroRibBuilder.
SkinFaceCollector
¶ Returns the skin face collector
-------------------------------------
Getter Method
Signature
SkinFaceCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
Thickness¶
-
AeroRibBuilder.
Thickness
¶ Returns the thickness
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ThicknessDimensionType¶
-
AeroRibBuilder.
ThicknessDimensionType
¶ Returns or sets the thickness dimension type
-------------------------------------
Getter Method
Signature
ThicknessDimensionType()
Returns: Return type: NXOpen.Features.AeroRibBuilderThicknessDimensionOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessDimensionType(thicknessDimensionType)
Parameters: thicknessDimensionType ( NXOpen.Features.AeroRibBuilderThicknessDimensionOptions
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Method Detail¶
Validate¶
-
AeroRibBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.