TransientText Class¶
-
class
NXOpen.Display.
TransientText
¶ Bases:
NXOpen.TransientObject
Represents temporary text strings which can be used for Temporary Display
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the index of the color to be used to display the transient text. |
FontStyle | Returns or sets the style of font to be used to display the transient text. |
ReferencePositionType | Returns or sets the position of the text relative to positions on the text box |
ScreenTextSize | Returns or sets the approximate size of the text (small, mendium, large) as measured on the graphics screen. |
Methods¶
Method | Description |
---|---|
AddTextString | Adds a text string to the TransientText object. |
DisplayTemporaryAbsRotScreenSizeGeometry | Displays text as temporary display using screen geometry but with rotation defined in absolute space. |
DisplayTemporaryAbsoluteGeometry | Displays text as temporary display using absolute geometry. |
DisplayTemporaryScreenGeometry | Displays text as temporary display using screen geometry. |
Dispose | Frees the object from memory. |
GetAbsoluteTextSize | Returns the size of the text, in absolute coordinate, in units of the displayed part. |
SetAbsoluteTextSize | Sets the size of the text, in absolute coordinates, in units of the displayed part. |
Enumerations¶
TransientTextStandardTextRef Enumeration | This enumerated type specifies the type of reference point used in the text box for standard_text methods. |
TransientTextTextSize Enumeration | Provides a way to specify the size of the desired text, as small, medium or large (normal is a synonym for medium). |
TransientTextViewType Enumeration | the view or views in which the transient text is to be displayed. |
Property Detail¶
Color¶
-
TransientText.
Color
¶ Returns or sets the index of the color to be used to display the transient text.
If not specified, the System Color will be used.
-------------------------------------
Getter Method
Signature
Color()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(colorIndex)
Parameters: colorIndex (int) – New in version NX8.0.0.
License requirements: None.
FontStyle¶
-
TransientText.
FontStyle
¶ Returns or sets the style of font to be used to display the transient text.
Every text font has at least one style. To determine which styles a font has, use UF_UGFONT_ask_font_styles. If not specified, the default font style for the font will be used.
-------------------------------------
Getter Method
Signature
FontStyle()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FontStyle(fontStyle)
Parameters: fontStyle (str) – New in version NX8.0.0.
License requirements: None.
ReferencePositionType¶
-
TransientText.
ReferencePositionType
¶ Returns or sets the position of the text relative to positions on the text box
-------------------------------------
Getter Method
Signature
ReferencePositionType()
Returns: Return type: NXOpen.Display.TransientTextStandardTextRef
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePositionType(referencePositionType)
Parameters: referencePositionType ( NXOpen.Display.TransientTextStandardTextRef
) –New in version NX8.0.0.
License requirements: None.
ScreenTextSize¶
-
TransientText.
ScreenTextSize
¶ Returns or sets the approximate size of the text (small, mendium, large) as measured on the graphics screen.
This property is not used by
Display.TransientText.DisplayTemporaryAbsoluteGeometry
.-------------------------------------
Getter Method
Signature
ScreenTextSize()
Returns: Return type: NXOpen.Display.TransientTextTextSize
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScreenTextSize(textSize)
Parameters: textSize ( NXOpen.Display.TransientTextTextSize
) –New in version NX8.0.0.
License requirements: None.
Method Detail¶
AddTextString¶
-
TransientText.
AddTextString
¶ Adds a text string to the TransientText object.
A TransientText object may have one or more text strings. If an attempt is made to display a TransientText object with zero text strings, an error will be returned.
Signature
AddTextString(textString)
Parameters: textString (str) – New in version NX8.0.0.
License requirements: None.
DisplayTemporaryAbsRotScreenSizeGeometry¶
-
TransientText.
DisplayTemporaryAbsRotScreenSizeGeometry
¶ Displays text as temporary display using screen geometry but with rotation defined in absolute space.
The text will be displayed on the XY plane of the absolute coordinate system. Insure that you have set all needed properties before using this method. This method is not supported for 2D output such as CGM.
Signature
DisplayTemporaryAbsRotScreenSizeGeometry(fontIndex, view, viewType, object, position)
Parameters: - fontIndex (int) – The index of the font to be used. This may be 0, which means to use the default font.
- view (
NXOpen.View
) – The view in which to display the text. This may be None, in which case the viewType argument is used. - viewType (
NXOpen.Display.TransientTextViewType
) – Used only when view is None. - object (
NXOpen.DisplayableObject
) – May be None, in which case the text will be drawn at the given position. If not None, draw the text at the attention point of object. - position (
NXOpen.Point3d
) – In Absolute Coordinates
New in version NX8.0.0.
License requirements: None.
DisplayTemporaryAbsoluteGeometry¶
-
TransientText.
DisplayTemporaryAbsoluteGeometry
¶ Displays text as temporary display using absolute geometry.
Insure that you have set all needed properties before using this method. Note that the text will be displayed on the Absolute XY plane.
Signature
DisplayTemporaryAbsoluteGeometry(fontIndex, view, viewType, object, position)
Parameters: - fontIndex (int) – The index of the font to be used. This may be 0, which means to use the default font.
- view (
NXOpen.View
) – The view in which to display the text. This may be None, in which case the viewType argument is used. - viewType (
NXOpen.Display.TransientTextViewType
) – Used only when view is None. - object (
NXOpen.DisplayableObject
) – May be None, in which case the text will be drawn at the given position. If not None, draw the text at the attention point of object. - position (
NXOpen.Point3d
) – In Absolute Coordinates
New in version NX8.0.0.
License requirements: None.
DisplayTemporaryScreenGeometry¶
-
TransientText.
DisplayTemporaryScreenGeometry
¶ Displays text as temporary display using screen geometry.
Insure that you have set all needed properties before using this method. This method is not supported for 2D output such as CGM. Note that the text will be displayed on the Absolute XY plane.
Signature
DisplayTemporaryScreenGeometry(fontIndex, view, viewType, object, position)
Parameters: - fontIndex (int) – The index of the font to be used. This may be 0, which means to use the default font.
- view (
NXOpen.View
) – The view in which to display the text. This may be None, in which case the viewType argument is used. - viewType (
NXOpen.Display.TransientTextViewType
) – Used only when view is None. - object (
NXOpen.DisplayableObject
) – May be None, in which case the text will be drawn at the given position. If not None, draw the text at the attention point of object. - position (
NXOpen.Point3d
) – In Absolute Coordinates
New in version NX8.0.0.
License requirements: None.
Dispose¶
-
TransientText.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.0.0.
License requirements: None.
GetAbsoluteTextSize¶
-
TransientText.
GetAbsoluteTextSize
¶ Returns the size of the text, in absolute coordinate, in units of the displayed part.
These values are only only used by
Display.TransientText.DisplayTemporaryAbsoluteGeometry
.Signature
GetAbsoluteTextSize()
Returns: a tuple Return type: A tuple consisting of (glyphWidth, glyphHeight). glyphWidth is a float. glyphHeight is a float. New in version NX8.0.0.
License requirements: None.
SetAbsoluteTextSize¶
-
TransientText.
SetAbsoluteTextSize
¶ Sets the size of the text, in absolute coordinates, in units of the displayed part.
These values are only used by
Display.TransientText.DisplayTemporaryAbsoluteGeometry
.Signature
SetAbsoluteTextSize(glyphWidth, glyphHeight)
Parameters: - glyphWidth (float) –
- glyphHeight (float) –
New in version NX8.0.0.
License requirements: None.