RotaryFinishGeomBuilder Class¶
-
class
NXOpen.CAM.
RotaryFinishGeomBuilder
¶ Bases:
NXOpen.CAM.FeatureGeomBuilder
Represents a rotary finish geometry builder.
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateRotaryFinishGeometryBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AxisOfRotation | Returns or sets the axis of rotation mode |
BlankOffsetBuilder | Returns the blank offset (inheritable double) |
CheckOffsetBuilder | Returns the check offset (inheritable double) |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
GeometryCiBuilder | Returns the geometry builder |
LayoutCiBuilder | Returns the save/layer layout builder |
OptimizationMethod | Returns or sets the optim method |
PartAxisBuilder | Returns the part axis builder |
PartAxisPoint | Returns or sets the part axis point |
PartAxisVector | Returns or sets the part axis vector |
PartMaterialBuilder | Returns or sets the part material |
PartOffsetBuilder | Returns the part offset (inheritable double) |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TrimOffsetBuilder | Returns the trim offset (inheritable double) |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMaterial | Get part material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set part material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RotaryFinishGeomBuilderPartAxisOfRotationTypes Enumeration | Available types for Part Axis of Rotation |
Property Detail¶
AxisOfRotation¶
-
RotaryFinishGeomBuilder.
AxisOfRotation
¶ Returns or sets the axis of rotation mode
-------------------------------------
Getter Method
Signature
AxisOfRotation()
Returns: the axis of rotation mode Return type: NXOpen.CAM.RotaryFinishGeomBuilderPartAxisOfRotationTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisOfRotation(axis)
Parameters: axis ( NXOpen.CAM.RotaryFinishGeomBuilderPartAxisOfRotationTypes
) – the axis of rotation modeNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
PartAxisBuilder¶
-
RotaryFinishGeomBuilder.
PartAxisBuilder
¶ Returns the part axis builder
-------------------------------------
Getter Method
Signature
PartAxisBuilder()
Returns: Return type: NXOpen.CAM.PartAxisBuilder
New in version NX9.0.0.
License requirements: None.
PartAxisPoint¶
-
RotaryFinishGeomBuilder.
PartAxisPoint
¶ Returns or sets the part axis point
-------------------------------------
Getter Method
Signature
PartAxisPoint()
Returns: the part axis point Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartAxisPoint(point)
Parameters: point ( NXOpen.Point
) – the part axis pointNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
PartAxisVector¶
-
RotaryFinishGeomBuilder.
PartAxisVector
¶ Returns or sets the part axis vector
-------------------------------------
Getter Method
Signature
PartAxisVector()
Returns: the part axis vector Return type: NXOpen.SmartObject
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartAxisVector(vector)
Parameters: vector ( NXOpen.SmartObject
) – the part axis vectorNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
RotaryFinishGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.