PartAxisBuilder Class¶
-
class
NXOpen.CAM.
PartAxisBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a part axis builder.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AxisOfRotation | Returns or sets the axis of rotation type |
PartAxisPoint | Returns or sets the part axis point |
PartAxisVector | Returns or sets the part axis vector |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
PartAxisBuilderPartAxisOfRotationTypes Enumeration | The types for part axis of rotation |
Property Detail¶
AxisOfRotation¶
-
PartAxisBuilder.
AxisOfRotation
¶ Returns or sets the axis of rotation type
-------------------------------------
Getter Method
Signature
AxisOfRotation()
Returns: the axis of rotation mode Return type: NXOpen.CAM.PartAxisBuilderPartAxisOfRotationTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisOfRotation(axis)
Parameters: axis ( NXOpen.CAM.PartAxisBuilderPartAxisOfRotationTypes
) – the axis of rotation modeNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
PartAxisPoint¶
-
PartAxisBuilder.
PartAxisPoint
¶ Returns or sets the part axis point
-------------------------------------
Getter Method
Signature
PartAxisPoint()
Returns: the part axis point Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartAxisPoint(point)
Parameters: point ( NXOpen.Point
) – the part axis pointNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
PartAxisVector¶
-
PartAxisBuilder.
PartAxisVector
¶ Returns or sets the part axis vector
-------------------------------------
Getter Method
Signature
PartAxisVector()
Returns: the part axis vector Return type: NXOpen.SmartObject
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartAxisVector(vector)
Parameters: vector ( NXOpen.SmartObject
) – the part axis vectorNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)