FeatureGeomBuilder Class¶
-
class
NXOpen.CAM.
FeatureGeomBuilder
¶ Bases:
NXOpen.CAM.NCGroupBuilder
Represents a FeatureGeom Builder
This is an abstract class, and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BlankOffsetBuilder | Returns the blank offset (inheritable double) |
CheckOffsetBuilder | Returns the check offset (inheritable double) |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
GeometryCiBuilder | Returns the geometry builder |
LayoutCiBuilder | Returns the save/layer layout builder |
OptimizationMethod | Returns or sets the optim method |
PartMaterialBuilder | Returns or sets the part material |
PartOffsetBuilder | Returns the part offset (inheritable double) |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TrimOffsetBuilder | Returns the trim offset (inheritable double) |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMaterial | Get part material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set part material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BlankOffsetBuilder¶
-
FeatureGeomBuilder.
BlankOffsetBuilder
¶ Returns the blank offset (inheritable double)
-------------------------------------
Getter Method
Signature
BlankOffsetBuilder()
Returns: The blank offset builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CheckOffsetBuilder¶
-
FeatureGeomBuilder.
CheckOffsetBuilder
¶ Returns the check offset (inheritable double)
-------------------------------------
Getter Method
Signature
CheckOffsetBuilder()
Returns: The check offset builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
GeometryCiBuilder¶
-
FeatureGeomBuilder.
GeometryCiBuilder
¶ Returns the geometry builder
-------------------------------------
Getter Method
Signature
GeometryCiBuilder()
Returns: The Geometry builder Return type: NXOpen.CAM.GeometryCiBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
LayoutCiBuilder¶
-
FeatureGeomBuilder.
LayoutCiBuilder
¶ Returns the save/layer layout builder
-------------------------------------
Getter Method
Signature
LayoutCiBuilder()
Returns: The save layer/layout builder Return type: NXOpen.CAM.LayoutCiBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
PartMaterialBuilder¶
-
FeatureGeomBuilder.
PartMaterialBuilder
¶ Returns or sets the part material
-------------------------------------
Getter Method
Signature
PartMaterialBuilder()
Returns: the part material tag Return type: NXOpen.NXObject
New in version NX5.0.0.
Deprecated since version NX8.0.2: Use method GetMaterialData instead.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
PartMaterialBuilder(partMaterial)
Parameters: partMaterial ( NXOpen.NXObject
) – the part material tagNew in version NX5.0.0.
Deprecated since version NX8.0.2: Use method SetMaterial instead.
License requirements: cam_base (“CAM BASE”)
PartOffsetBuilder¶
-
FeatureGeomBuilder.
PartOffsetBuilder
¶ Returns the part offset (inheritable double)
-------------------------------------
Getter Method
Signature
PartOffsetBuilder()
Returns: The part offset builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TrimOffsetBuilder¶
-
FeatureGeomBuilder.
TrimOffsetBuilder
¶ Returns the trim offset (inheritable double)
-------------------------------------
Getter Method
Signature
TrimOffsetBuilder()
Returns: The trim offset builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetMaterial¶
-
FeatureGeomBuilder.
GetMaterial
¶ Get part material
Signature
GetMaterial()
Returns: Return type: str New in version NX8.0.1.
License requirements: None.
GetMaterialData¶
-
FeatureGeomBuilder.
GetMaterialData
¶ Get material data
Signature
GetMaterialData()
Returns: a tuple Return type: A tuple consisting of (libRef, name, description, code, hardness). libRef is a str. name is a str. description is a str. code is a str. hardness is a str. New in version NX8.0.2.
License requirements: None.
SetMaterial¶
-
FeatureGeomBuilder.
SetMaterial
¶ Set part material
Signature
SetMaterial(libRef)
Parameters: libRef (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.1.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
FeatureGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.