InspectionAlignmentBuilder Class¶
-
class
NXOpen.CAM.
InspectionAlignmentBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Alignment builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionAlignmentBuilder
New in version NX7.5.2.
Properties¶
Property | Description |
---|---|
AlignOpName | Returns or sets the align op name |
AlignType | Returns or sets the alignment type |
ChannelName | Returns or sets the channel’s name |
ComponentSelection | Returns the component selection |
CsysPick | Returns or sets the csys pick |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FailGroupName | Returns or sets the fail group name |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
IterAvailSelect | Returns the iter avail select |
IterConvergeVar | Returns or sets the iter converge variable |
IterDev | Returns or sets the iter deviation |
IterDevType | Returns or sets the iter deviation type |
IterGroupName | Returns or sets the iter group name |
IterMax | Returns or sets the iter max iterations |
LayoutAndLayer | Returns the Layer and Layout |
LocateAvailSelect | Returns the locate avail select |
LocateXrot | Returns or sets the locate xrot |
LocateXtrans | Returns or sets the locate xtrans |
LocateYrot | Returns or sets the locate yrot |
LocateYtrans | Returns or sets the locate ytrans |
LocateZrot | Returns or sets the locate zrot |
LocateZtrans | Returns or sets the locate ztrans |
MotionOutputBuilder | Returns the motion output builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PcsName | Returns or sets the pcs name |
PriDatLetter | Returns or sets the pri dat letter |
PriDirection | Returns or sets the pri direction |
PriXorigin | Returns or sets the pri xorigin |
PriYorigin | Returns or sets the pri yorigin |
PriZorigin | Returns or sets the pri zorigin |
RecallCsys | Returns or sets the recall csys |
RecallDid | Returns or sets the recall device id |
RecallExtName | Returns or sets the recall external name |
RecallIntName | Returns or sets the recall internal name |
RecallState | Returns or sets the recall state |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
RotateTableAngle | Returns or sets the angle to rotate table |
RotateTableAngularDeviation | Returns or sets the rotate table angular deviation |
RotateTableDirection | Returns or sets the rotate table direction |
RotateTableFeature | Returns or sets the feature used to position table |
RotateTableFeatureSelect | Returns the feature selected to position table |
RotateTableMethod | Returns or sets the rotate table method |
RotateTableName | Returns or sets the name of rotary table to rotate |
RotateTablePcsUpdateOption | Returns or sets the rotate table pcs update |
RotationAngle | Returns or sets the rot angle |
RotationAxis | Returns or sets the rot axis |
RotationDatumLetter | Returns or sets the rot datum letter |
RotationDirection | Returns or sets the rot dir |
RotationFeature | Returns or sets the rot feature |
RotationFeatureSelect | Returns the rot feature select |
RotationMethod | Returns or sets the rot method |
SafeClearance | Returns the safe clearance builder |
SaveDid | Returns or sets the save device id |
SavePcsLabel | Returns or sets the save pcs label |
SaveState | Returns or sets the save state |
SecDatLetter | Returns or sets the sec dat letter |
SecDirection | Returns or sets the sec direction |
SecXorigin | Returns or sets the sec xorigin |
SecYorigin | Returns or sets the sec yorigin |
SecZorigin | Returns or sets the sec zorigin |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TerDatLetter | Returns or sets the ter dat letter |
TerDirection | Returns or sets the ter xdirection |
TerXorigin | Returns or sets the ter xorigin |
TerYorigin | Returns or sets the ter yorigin |
TerZorigin | Returns or sets the ter zorigin |
ToolChangeSetting | Returns the tool change builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
WcsOrientOption | Returns or sets the WCS Orient option |
XtDatumLetter | Returns or sets the xt datum letter |
XtDistance | Returns or sets the xt distance |
XtFeature | Returns or sets the xt feature |
XtFeatureSelect | Returns the xt feature select |
XtMethod | Returns or sets the xt method |
YtDatumLetter | Returns or sets the yt datum letter |
YtDistance | Returns or sets the yt distance |
YtFeature | Returns or sets the yt feature |
YtFeatureSelect | Returns the yt feature select |
YtMethod | Returns or sets the yt method |
ZtDatumLetter | Returns or sets the zt datum letter |
ZtDistance | Returns or sets the zt distance |
ZtFeature | Returns or sets the zt feature |
ZtFeatureSelect | Returns the zt feature select |
ZtMethod | Returns or sets the zt method |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AlignOpName¶
-
InspectionAlignmentBuilder.
AlignOpName
¶ Returns or sets the align op name
-------------------------------------
Getter Method
Signature
AlignOpName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignOpName(alignOpName)
Parameters: alignOpName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AlignType¶
-
InspectionAlignmentBuilder.
AlignType
¶ Returns or sets the alignment type
-------------------------------------
Getter Method
Signature
AlignType()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderAlignTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignType(alignType)
Parameters: alignType ( NXOpen.CAM.InspectionAlignmentBuilderAlignTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ComponentSelection¶
-
InspectionAlignmentBuilder.
ComponentSelection
¶ Returns the component selection
-------------------------------------
Getter Method
Signature
ComponentSelection()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX9.0.0.
License requirements: None.
CsysPick¶
-
InspectionAlignmentBuilder.
CsysPick
¶ Returns or sets the csys pick
-------------------------------------
Getter Method
Signature
CsysPick()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysPick(csysPick)
Parameters: csysPick ( NXOpen.CoordinateSystem
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FailGroupName¶
-
InspectionAlignmentBuilder.
FailGroupName
¶ Returns or sets the fail group name
-------------------------------------
Getter Method
Signature
FailGroupName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FailGroupName(failGroupName)
Parameters: failGroupName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterAvailSelect¶
-
InspectionAlignmentBuilder.
IterAvailSelect
¶ Returns the iter avail select
-------------------------------------
Getter Method
Signature
IterAvailSelect()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
IterConvergeVar¶
-
InspectionAlignmentBuilder.
IterConvergeVar
¶ Returns or sets the iter converge variable
-------------------------------------
Getter Method
Signature
IterConvergeVar()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterConvergeVar(iterConvergeVar)
Parameters: iterConvergeVar (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterDev¶
-
InspectionAlignmentBuilder.
IterDev
¶ Returns or sets the iter deviation
-------------------------------------
Getter Method
Signature
IterDev()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterDev(iterDev)
Parameters: iterDev (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterDevType¶
-
InspectionAlignmentBuilder.
IterDevType
¶ Returns or sets the iter deviation type
-------------------------------------
Getter Method
Signature
IterDevType()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderIterDevTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterDevType(iterDevType)
Parameters: iterDevType ( NXOpen.CAM.InspectionAlignmentBuilderIterDevTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterGroupName¶
-
InspectionAlignmentBuilder.
IterGroupName
¶ Returns or sets the iter group name
-------------------------------------
Getter Method
Signature
IterGroupName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterGroupName(iterGroupName)
Parameters: iterGroupName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterMax¶
-
InspectionAlignmentBuilder.
IterMax
¶ Returns or sets the iter max iterations
-------------------------------------
Getter Method
Signature
IterMax()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterMax(iterMax)
Parameters: iterMax (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateAvailSelect¶
-
InspectionAlignmentBuilder.
LocateAvailSelect
¶ Returns the locate avail select
-------------------------------------
Getter Method
Signature
LocateAvailSelect()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
LocateXrot¶
-
InspectionAlignmentBuilder.
LocateXrot
¶ Returns or sets the locate xrot
-------------------------------------
Getter Method
Signature
LocateXrot()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateXrot(locateXrot)
Parameters: locateXrot (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateXtrans¶
-
InspectionAlignmentBuilder.
LocateXtrans
¶ Returns or sets the locate xtrans
-------------------------------------
Getter Method
Signature
LocateXtrans()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateXtrans(locateXtrans)
Parameters: locateXtrans (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateYrot¶
-
InspectionAlignmentBuilder.
LocateYrot
¶ Returns or sets the locate yrot
-------------------------------------
Getter Method
Signature
LocateYrot()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateYrot(locateYrot)
Parameters: locateYrot (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateYtrans¶
-
InspectionAlignmentBuilder.
LocateYtrans
¶ Returns or sets the locate ytrans
-------------------------------------
Getter Method
Signature
LocateYtrans()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateYtrans(locateYtrans)
Parameters: locateYtrans (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateZrot¶
-
InspectionAlignmentBuilder.
LocateZrot
¶ Returns or sets the locate zrot
-------------------------------------
Getter Method
Signature
LocateZrot()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateZrot(locateZrot)
Parameters: locateZrot (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateZtrans¶
-
InspectionAlignmentBuilder.
LocateZtrans
¶ Returns or sets the locate ztrans
-------------------------------------
Getter Method
Signature
LocateZtrans()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateZtrans(locateZtrans)
Parameters: locateZtrans (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PcsName¶
-
InspectionAlignmentBuilder.
PcsName
¶ Returns or sets the pcs name
-------------------------------------
Getter Method
Signature
PcsName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PcsName(pcsName)
Parameters: pcsName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriDatLetter¶
-
InspectionAlignmentBuilder.
PriDatLetter
¶ Returns or sets the pri dat letter
-------------------------------------
Getter Method
Signature
PriDatLetter()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriDatLetter(priDatLetter)
Parameters: priDatLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriDirection¶
-
InspectionAlignmentBuilder.
PriDirection
¶ Returns or sets the pri direction
-------------------------------------
Getter Method
Signature
PriDirection()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriDirection(priDirection)
Parameters: priDirection ( NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriXorigin¶
-
InspectionAlignmentBuilder.
PriXorigin
¶ Returns or sets the pri xorigin
-------------------------------------
Getter Method
Signature
PriXorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriXorigin(priXorigin)
Parameters: priXorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriYorigin¶
-
InspectionAlignmentBuilder.
PriYorigin
¶ Returns or sets the pri yorigin
-------------------------------------
Getter Method
Signature
PriYorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriYorigin(priYorigin)
Parameters: priYorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriZorigin¶
-
InspectionAlignmentBuilder.
PriZorigin
¶ Returns or sets the pri zorigin
-------------------------------------
Getter Method
Signature
PriZorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriZorigin(priZorigin)
Parameters: priZorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallCsys¶
-
InspectionAlignmentBuilder.
RecallCsys
¶ Returns or sets the recall csys
-------------------------------------
Getter Method
Signature
RecallCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallCsys(recallCsys)
Parameters: recallCsys ( NXOpen.CoordinateSystem
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallDid¶
-
InspectionAlignmentBuilder.
RecallDid
¶ Returns or sets the recall device id
-------------------------------------
Getter Method
Signature
RecallDid()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallDid(recallDid)
Parameters: recallDid (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallExtName¶
-
InspectionAlignmentBuilder.
RecallExtName
¶ Returns or sets the recall external name
-------------------------------------
Getter Method
Signature
RecallExtName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallExtName(recallExtName)
Parameters: recallExtName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallIntName¶
-
InspectionAlignmentBuilder.
RecallIntName
¶ Returns or sets the recall internal name
-------------------------------------
Getter Method
Signature
RecallIntName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallIntName(recallIntName)
Parameters: recallIntName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallState¶
-
InspectionAlignmentBuilder.
RecallState
¶ Returns or sets the recall state
-------------------------------------
Getter Method
Signature
RecallState()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRecallStates
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallState(recallState)
Parameters: recallState ( NXOpen.CAM.InspectionAlignmentBuilderRecallStates
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableAngle¶
-
InspectionAlignmentBuilder.
RotateTableAngle
¶ Returns or sets the angle to rotate table
-------------------------------------
Getter Method
Signature
RotateTableAngle()
Returns: Return type: float New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableAngle(angle)
Parameters: angle (float) – New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableAngularDeviation¶
-
InspectionAlignmentBuilder.
RotateTableAngularDeviation
¶ Returns or sets the rotate table angular deviation
-------------------------------------
Getter Method
Signature
RotateTableAngularDeviation()
Returns: Return type: float New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableAngularDeviation(fz)
Parameters: fz (float) – New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableDirection¶
-
InspectionAlignmentBuilder.
RotateTableDirection
¶ Returns or sets the rotate table direction
-------------------------------------
Getter Method
Signature
RotateTableDirection()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotateTableDirections
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableDirection(direction)
Parameters: direction ( NXOpen.CAM.InspectionAlignmentBuilderRotateTableDirections
) –New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableFeature¶
-
InspectionAlignmentBuilder.
RotateTableFeature
¶ Returns or sets the feature used to position table
-------------------------------------
Getter Method
Signature
RotateTableFeature()
Returns: Return type: str New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableFeature(rotateTableFeature)
Parameters: rotateTableFeature (str) – New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableFeatureSelect¶
-
InspectionAlignmentBuilder.
RotateTableFeatureSelect
¶ Returns the feature selected to position table
-------------------------------------
Getter Method
Signature
RotateTableFeatureSelect()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.2.
License requirements: None.
RotateTableMethod¶
-
InspectionAlignmentBuilder.
RotateTableMethod
¶ Returns or sets the rotate table method
-------------------------------------
Getter Method
Signature
RotateTableMethod()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotateTableMethods
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableMethod(method)
Parameters: method ( NXOpen.CAM.InspectionAlignmentBuilderRotateTableMethods
) –New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableName¶
-
InspectionAlignmentBuilder.
RotateTableName
¶ Returns or sets the name of rotary table to rotate
-------------------------------------
Getter Method
Signature
RotateTableName()
Returns: Return type: str New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableName(tableName)
Parameters: tableName (str) – New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTablePcsUpdateOption¶
-
InspectionAlignmentBuilder.
RotateTablePcsUpdateOption
¶ Returns or sets the rotate table pcs update
-------------------------------------
Getter Method
Signature
RotateTablePcsUpdateOption()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotateTablePcsUpdateOptions
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTablePcsUpdateOption(pcsUpdate)
Parameters: pcsUpdate ( NXOpen.CAM.InspectionAlignmentBuilderRotateTablePcsUpdateOptions
) –New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationAngle¶
-
InspectionAlignmentBuilder.
RotationAngle
¶ Returns or sets the rot angle
-------------------------------------
Getter Method
Signature
RotationAngle()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationAngle(rotationAngle)
Parameters: rotationAngle (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationAxis¶
-
InspectionAlignmentBuilder.
RotationAxis
¶ Returns or sets the rot axis
-------------------------------------
Getter Method
Signature
RotationAxis()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotationAxisOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationAxis(rotationAxis)
Parameters: rotationAxis ( NXOpen.CAM.InspectionAlignmentBuilderRotationAxisOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationDatumLetter¶
-
InspectionAlignmentBuilder.
RotationDatumLetter
¶ Returns or sets the rot datum letter
-------------------------------------
Getter Method
Signature
RotationDatumLetter()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationDatumLetter(rotationDatumLetter)
Parameters: rotationDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationDirection¶
-
InspectionAlignmentBuilder.
RotationDirection
¶ Returns or sets the rot dir
-------------------------------------
Getter Method
Signature
RotationDirection()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotationDirections
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationDirection(rotationDirection)
Parameters: rotationDirection ( NXOpen.CAM.InspectionAlignmentBuilderRotationDirections
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationFeature¶
-
InspectionAlignmentBuilder.
RotationFeature
¶ Returns or sets the rot feature
-------------------------------------
Getter Method
Signature
RotationFeature()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationFeature(rotationFeature)
Parameters: rotationFeature (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationFeatureSelect¶
-
InspectionAlignmentBuilder.
RotationFeatureSelect
¶ Returns the rot feature select
-------------------------------------
Getter Method
Signature
RotationFeatureSelect()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
RotationMethod¶
-
InspectionAlignmentBuilder.
RotationMethod
¶ Returns or sets the rot method
-------------------------------------
Getter Method
Signature
RotationMethod()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotationMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationMethod(rotationMethod)
Parameters: rotationMethod ( NXOpen.CAM.InspectionAlignmentBuilderRotationMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDid¶
-
InspectionAlignmentBuilder.
SaveDid
¶ Returns or sets the save device id
-------------------------------------
Getter Method
Signature
SaveDid()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDid(saveDid)
Parameters: saveDid (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SavePcsLabel¶
-
InspectionAlignmentBuilder.
SavePcsLabel
¶ Returns or sets the save pcs label
-------------------------------------
Getter Method
Signature
SavePcsLabel()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SavePcsLabel(savePcsLabel)
Parameters: savePcsLabel (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveState¶
-
InspectionAlignmentBuilder.
SaveState
¶ Returns or sets the save state
-------------------------------------
Getter Method
Signature
SaveState()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderSaveStates
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveState(saveState)
Parameters: saveState ( NXOpen.CAM.InspectionAlignmentBuilderSaveStates
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecDatLetter¶
-
InspectionAlignmentBuilder.
SecDatLetter
¶ Returns or sets the sec dat letter
-------------------------------------
Getter Method
Signature
SecDatLetter()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecDatLetter(secDatLetter)
Parameters: secDatLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecDirection¶
-
InspectionAlignmentBuilder.
SecDirection
¶ Returns or sets the sec direction
-------------------------------------
Getter Method
Signature
SecDirection()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecDirection(secDirection)
Parameters: secDirection ( NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecXorigin¶
-
InspectionAlignmentBuilder.
SecXorigin
¶ Returns or sets the sec xorigin
-------------------------------------
Getter Method
Signature
SecXorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecXorigin(secXorigin)
Parameters: secXorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecYorigin¶
-
InspectionAlignmentBuilder.
SecYorigin
¶ Returns or sets the sec yorigin
-------------------------------------
Getter Method
Signature
SecYorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecYorigin(secYorigin)
Parameters: secYorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecZorigin¶
-
InspectionAlignmentBuilder.
SecZorigin
¶ Returns or sets the sec zorigin
-------------------------------------
Getter Method
Signature
SecZorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecZorigin(secZorigin)
Parameters: secZorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerDatLetter¶
-
InspectionAlignmentBuilder.
TerDatLetter
¶ Returns or sets the ter dat letter
-------------------------------------
Getter Method
Signature
TerDatLetter()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerDatLetter(terDatLetter)
Parameters: terDatLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerDirection¶
-
InspectionAlignmentBuilder.
TerDirection
¶ Returns or sets the ter xdirection
-------------------------------------
Getter Method
Signature
TerDirection()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerDirection(terDirection)
Parameters: terDirection ( NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerXorigin¶
-
InspectionAlignmentBuilder.
TerXorigin
¶ Returns or sets the ter xorigin
-------------------------------------
Getter Method
Signature
TerXorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerXorigin(terXorigin)
Parameters: terXorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerYorigin¶
-
InspectionAlignmentBuilder.
TerYorigin
¶ Returns or sets the ter yorigin
-------------------------------------
Getter Method
Signature
TerYorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerYorigin(terYorigin)
Parameters: terYorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerZorigin¶
-
InspectionAlignmentBuilder.
TerZorigin
¶ Returns or sets the ter zorigin
-------------------------------------
Getter Method
Signature
TerZorigin()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerZorigin(terZorigin)
Parameters: terZorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
WcsOrientOption¶
-
InspectionAlignmentBuilder.
WcsOrientOption
¶ Returns or sets the WCS Orient option
-------------------------------------
Getter Method
Signature
WcsOrientOption()
Returns: Return type: bool New in version NX8.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
WcsOrientOption(wcsOrientOption)
Parameters: wcsOrientOption (bool) – New in version NX8.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XtDatumLetter¶
-
InspectionAlignmentBuilder.
XtDatumLetter
¶ Returns or sets the xt datum letter
-------------------------------------
Getter Method
Signature
XtDatumLetter()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XtDatumLetter(xtDatumLetter)
Parameters: xtDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XtDistance¶
-
InspectionAlignmentBuilder.
XtDistance
¶ Returns or sets the xt distance
-------------------------------------
Getter Method
Signature
XtDistance()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XtDistance(xtDistance)
Parameters: xtDistance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XtFeature¶
-
InspectionAlignmentBuilder.
XtFeature
¶ Returns or sets the xt feature
-------------------------------------
Getter Method
Signature
XtFeature()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XtFeature(xtFeature)
Parameters: xtFeature (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XtFeatureSelect¶
-
InspectionAlignmentBuilder.
XtFeatureSelect
¶ Returns the xt feature select
-------------------------------------
Getter Method
Signature
XtFeatureSelect()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
XtMethod¶
-
InspectionAlignmentBuilder.
XtMethod
¶ Returns or sets the xt method
-------------------------------------
Getter Method
Signature
XtMethod()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderXtMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XtMethod(xtMethod)
Parameters: xtMethod ( NXOpen.CAM.InspectionAlignmentBuilderXtMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YtDatumLetter¶
-
InspectionAlignmentBuilder.
YtDatumLetter
¶ Returns or sets the yt datum letter
-------------------------------------
Getter Method
Signature
YtDatumLetter()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YtDatumLetter(ytDatumLetter)
Parameters: ytDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YtDistance¶
-
InspectionAlignmentBuilder.
YtDistance
¶ Returns or sets the yt distance
-------------------------------------
Getter Method
Signature
YtDistance()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YtDistance(ytDistance)
Parameters: ytDistance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YtFeature¶
-
InspectionAlignmentBuilder.
YtFeature
¶ Returns or sets the yt feature
-------------------------------------
Getter Method
Signature
YtFeature()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YtFeature(ytFeature)
Parameters: ytFeature (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YtFeatureSelect¶
-
InspectionAlignmentBuilder.
YtFeatureSelect
¶ Returns the yt feature select
-------------------------------------
Getter Method
Signature
YtFeatureSelect()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
YtMethod¶
-
InspectionAlignmentBuilder.
YtMethod
¶ Returns or sets the yt method
-------------------------------------
Getter Method
Signature
YtMethod()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderYtMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YtMethod(ytMethod)
Parameters: ytMethod ( NXOpen.CAM.InspectionAlignmentBuilderYtMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZtDatumLetter¶
-
InspectionAlignmentBuilder.
ZtDatumLetter
¶ Returns or sets the zt datum letter
-------------------------------------
Getter Method
Signature
ZtDatumLetter()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZtDatumLetter(ztDatumLetter)
Parameters: ztDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZtDistance¶
-
InspectionAlignmentBuilder.
ZtDistance
¶ Returns or sets the zt distance
-------------------------------------
Getter Method
Signature
ZtDistance()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZtDistance(ztDistance)
Parameters: ztDistance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZtFeature¶
-
InspectionAlignmentBuilder.
ZtFeature
¶ Returns or sets the zt feature
-------------------------------------
Getter Method
Signature
ZtFeature()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZtFeature(ztFeature)
Parameters: ztFeature (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZtFeatureSelect¶
-
InspectionAlignmentBuilder.
ZtFeatureSelect
¶ Returns the zt feature select
-------------------------------------
Getter Method
Signature
ZtFeatureSelect()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
ZtMethod¶
-
InspectionAlignmentBuilder.
ZtMethod
¶ Returns or sets the zt method
-------------------------------------
Getter Method
Signature
ZtMethod()
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderZtMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZtMethod(ztMethod)
Parameters: ztMethod ( NXOpen.CAM.InspectionAlignmentBuilderZtMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
InspectionAlignmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.