InspectionAlignmentBuilderAlignmentDirections Enumeration¶
NXOpen.CAM.InspectionAlignmentBuilder.AlignmentDirections is an alias for NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
-
class
NXOpen.CAM.
InspectionAlignmentBuilderAlignmentDirections
¶ Bases:
object
Alignment directions of datum features
Enum Members
Enum Member Enum Member Description None No alignment direction specifiedPxdir Align feature in the positive X directionPydir Align feature in the positive Y directionPzdir Align feature in the positive Z directionMxdir Align feature in the negitive X directionMydir Align feature in the negitive Y directionMzdir Align feature in the negitive Z direction-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-