InspectionAlignmentBuilderRotationDirections Enumeration¶
NXOpen.CAM.InspectionAlignmentBuilder.RotationDirections is an alias for NXOpen.CAM.InspectionAlignmentBuilderRotationDirections
-
class
NXOpen.CAM.
InspectionAlignmentBuilderRotationDirections
¶ Bases:
object
Direction to rotate about
Enum Members
Enum Member Enum Member Description Pxdir Rotate in the positive X directionPydir Rotate in the positive Y directionPzdir Rotate in the positive Z directionMxdir Rotate in the negitive X directionMydir Rotate in the negitive Y directionMzdir Rotate in the negitive Z direction-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-