DiagramDisplayStyles Class¶
-
class
NXOpen.CAE.Xyplot.
DiagramDisplayStyles
¶ Bases:
NXOpen.TaggedObject
Manages the diagram display styles.
Not support KF.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
StyleCount | Returns the style count |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetBarStyleSetting | Gets the bar display style. |
GetGraphStyle | Gets the graph style. |
GetLineStyleSetting | Gets the line display style. |
GetPlateStyleSetting | Gets the plate display style. |
GetScatterStyleSetting | Gets the scatter display style. |
GetSurfaceStyleSetting | Gets the surface display style. |
SetGraphStyle | Sets the graph style. |
Property Detail¶
Method Detail¶
GetBarStyleSetting¶
-
DiagramDisplayStyles.
GetBarStyleSetting
¶ Gets the bar display style.
The style index must be greater than or equal to 0 and less than
CAE.Xyplot.DiagramDisplayStyles.StyleCount
.Signature
GetBarStyleSetting(styleIndex)
Parameters: styleIndex (int) – Style index Returns: Bar style Return type: NXOpen.CAE.Xyplot.BaseBarStyleSetting
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetGraphStyle¶
-
DiagramDisplayStyles.
GetGraphStyle
¶ Gets the graph style.
The style index must be greater than or equal to 0 and less than
CAE.Xyplot.DiagramDisplayStyles.StyleCount
.Signature
GetGraphStyle(styleIndex)
Parameters: styleIndex (int) – Style index Returns: Graph style Return type: NXOpen.CAE.Xyplot.GraphStyle
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetLineStyleSetting¶
-
DiagramDisplayStyles.
GetLineStyleSetting
¶ Gets the line display style.
The style index must be greater than or equal to 0 and less than
CAE.Xyplot.DiagramDisplayStyles.StyleCount
.Signature
GetLineStyleSetting(styleIndex)
Parameters: styleIndex (int) – Style index Returns: Line style Return type: NXOpen.CAE.Xyplot.BaseLineStyleSetting
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetPlateStyleSetting¶
-
DiagramDisplayStyles.
GetPlateStyleSetting
¶ Gets the plate display style.
The style index must be greater than or equal to 0 and less than
CAE.Xyplot.DiagramDisplayStyles.StyleCount
.Signature
GetPlateStyleSetting(styleIndex)
Parameters: styleIndex (int) – Style index Returns: Plate style Return type: NXOpen.CAE.Xyplot.BasePlateStyleSetting
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetScatterStyleSetting¶
-
DiagramDisplayStyles.
GetScatterStyleSetting
¶ Gets the scatter display style.
The style index must be greater than or equal to 0 and less than
CAE.Xyplot.DiagramDisplayStyles.StyleCount
.Signature
GetScatterStyleSetting(styleIndex)
Parameters: styleIndex (int) – Style index Returns: Scatter style Return type: NXOpen.CAE.Xyplot.ScatterStyleSetting
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetSurfaceStyleSetting¶
-
DiagramDisplayStyles.
GetSurfaceStyleSetting
¶ Gets the surface display style.
The style index must be greater than or equal to 0 and less than
CAE.Xyplot.DiagramDisplayStyles.StyleCount
.Signature
GetSurfaceStyleSetting(styleIndex)
Parameters: styleIndex (int) – Style index Returns: Surface style Return type: NXOpen.CAE.Xyplot.SurfaceStyleSetting
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
SetGraphStyle¶
-
DiagramDisplayStyles.
SetGraphStyle
¶ Sets the graph style.
The style index must be greater than or equal to 0 and less than
CAE.Xyplot.DiagramDisplayStyles.StyleCount
.Signature
SetGraphStyle(styleIndex, graphStyle)
Parameters: - styleIndex (int) – Style index
- graphStyle (
NXOpen.CAE.Xyplot.GraphStyle
) – Graph style
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)