GraphStyle Enumeration¶
-
class
NXOpen.CAE.Xyplot.
GraphStyle
¶ Bases:
object
Represents the plot graph style Enum Members
Enum Member Enum Member Description Line Option to display plot in curve styleBar Option to display plot in bar stylePlate Option to display plot in plate styleSurface Option to display plot in surface styleScatter Option to display plot in scatter style-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-