ScatterStyleSetting Class¶
-
class
NXOpen.CAE.Xyplot.
ScatterStyleSetting
¶ Bases:
NXOpen.CAE.Xyplot.BaseSymbolStyleSetting
Represents the scatter display style.
Call
CAE.Xyplot.IDisplayStyle.CommitChange
to apply style changes to corresponding plot after it’s modified.Not support KF.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the point color |
Owner | Returns the owner style |
PointMarker | Returns or sets the point marker |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Property Detail¶
Color¶
-
ScatterStyleSetting.
Color
¶ Returns or sets the point color
-------------------------------------
Getter Method
Signature
Color()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – New in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Owner¶
-
ScatterStyleSetting.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner()
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.