BaseSymbolStyleSetting Class¶
-
class
NXOpen.CAE.Xyplot.
BaseSymbolStyleSetting
¶ Bases:
NXOpen.TaggedObject
,NXOpen.CAE.Xyplot.IDisplayStyle
Represents the base symbol display style.
Call
CAE.Xyplot.IDisplayStyle.CommitChange
to apply style changes to corresponding plot after it’s modified.This is an abstract class.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Owner | Returns the owner style |
PointMarker | Returns or sets the point marker |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Property Detail¶
Owner¶
-
BaseSymbolStyleSetting.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner()
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.
PointMarker¶
-
BaseSymbolStyleSetting.
PointMarker
¶ Returns or sets the point marker
-------------------------------------
Getter Method
Signature
PointMarker()
Returns: Return type: NXOpen.CAE.Xyplot.PointMarker
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointMarker(pointMarker)
Parameters: pointMarker ( NXOpen.CAE.Xyplot.PointMarker
) –New in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)