SubsetCollection Class¶
-
class
NXOpen.Assemblies.
SubsetCollection
¶ Bases:
object
Represents a collection of subset.
To obtain an instance of this class, refer to
NXOpen.Assemblies.ComponentAssembly
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateAttributeSearchTermBuilder | Creates a NXOpen.Assemblies.AttributeSearchTermBuilder . |
CreateBoxSearchTermBuilder | Creates a NXOpen.Assemblies.BoxSearchTermBuilder . |
CreatePlaneSearchTermBuilder | Creates a NXOpen.Assemblies.PlaneSearchTermBuilder . |
CreatePositioningTaskBuilder | Creates a NXOpen.Assemblies.PositioningTaskBuilder @return |
CreateProximitySearchTermBuilder | Creates a NXOpen.Assemblies.ProximitySearchTermBuilder . |
CreateSubsetBuilder | Creates an NXOpen.Assemblies.SubsetBuilder @return |
Method Detail¶
CreateAttributeSearchTermBuilder¶
-
SubsetCollection.
CreateAttributeSearchTermBuilder
¶ Creates a
NXOpen.Assemblies.AttributeSearchTermBuilder
.Signature
CreateAttributeSearchTermBuilder(attributeSearchTerm)
Parameters: attributeSearchTerm ( NXOpen.Assemblies.AttributeSearchTerm
) –NXOpen.Assemblies.AttributeSearchTerm
to be edited, if None then create a new oneReturns: Return type: NXOpen.Assemblies.AttributeSearchTermBuilder
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
CreateBoxSearchTermBuilder¶
-
SubsetCollection.
CreateBoxSearchTermBuilder
¶ Creates a
NXOpen.Assemblies.BoxSearchTermBuilder
.Signature
CreateBoxSearchTermBuilder(boxSearchTerm)
Parameters: boxSearchTerm ( NXOpen.Assemblies.BoxSearchTerm
) –NXOpen.Assemblies.BoxSearchTerm
to be edited, if None then create a new oneReturns: Return type: NXOpen.Assemblies.BoxSearchTermBuilder
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
CreatePlaneSearchTermBuilder¶
-
SubsetCollection.
CreatePlaneSearchTermBuilder
¶ Creates a
NXOpen.Assemblies.PlaneSearchTermBuilder
.Signature
CreatePlaneSearchTermBuilder(planeSearchTerm)
Parameters: planeSearchTerm ( NXOpen.Assemblies.PlaneSearchTerm
) –NXOpen.Assemblies.PlaneSearchTerm
to be edited, if None then create a new oneReturns: Return type: NXOpen.Assemblies.PlaneSearchTermBuilder
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
CreatePositioningTaskBuilder¶
-
SubsetCollection.
CreatePositioningTaskBuilder
¶ Creates a
NXOpen.Assemblies.PositioningTaskBuilder
Signature
CreatePositioningTaskBuilder(positioningTask)
Parameters: positioningTask ( NXOpen.Assemblies.PositioningTask
) –Returns: Return type: NXOpen.Assemblies.PositioningTaskBuilder
New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
CreateProximitySearchTermBuilder¶
-
SubsetCollection.
CreateProximitySearchTermBuilder
¶ Creates a
NXOpen.Assemblies.ProximitySearchTermBuilder
.Signature
CreateProximitySearchTermBuilder(proximitySearchTerm)
Parameters: proximitySearchTerm ( NXOpen.Assemblies.ProximitySearchTerm
) –NXOpen.Assemblies.ProximitySearchTerm
to be edited, if None then create a new oneReturns: Return type: NXOpen.Assemblies.ProximitySearchTermBuilder
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
CreateSubsetBuilder¶
-
SubsetCollection.
CreateSubsetBuilder
¶ Creates an
NXOpen.Assemblies.SubsetBuilder
Signature
CreateSubsetBuilder(subset)
Parameters: subset ( NXOpen.Assemblies.Subset
) –NXOpen.Assemblies.Subset
to be edited, if None then create a new oneReturns: Return type: NXOpen.Assemblies.SubsetBuilder
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)