PlaneSearchTermBuilder Class¶
-
class
NXOpen.Assemblies.
PlaneSearchTermBuilder
¶ Bases:
NXOpen.Assemblies.SearchTermBuilder
A PlaneSearchTermBuilder is used to create or edit an
NXOpen.Assemblies.PlaneSearchTerm
.To create a new instance of this class, use
NXOpen.Assemblies.SubsetCollection.CreatePlaneSearchTermBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Displacement | Returns or sets the displacement of the plane from the origin. |
Normal | Returns or sets the normal of the plane. |
PlaneOverlapLogic | Returns or sets the plane overlap logic. |
PointOnPlane | Returns or sets the normal of the plane. |
SearchTermLogic | Returns or sets the search term logic. |
Tag | Returns the Tag for this object. |
TrueShapeRefinement | Returns or sets the true-shape refinement. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Displacement¶
-
PlaneSearchTermBuilder.
Displacement
¶ Returns or sets the displacement of the plane from the origin.
-------------------------------------
Getter Method
Signature
Displacement()
Returns: Return type: float New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
Displacement(displacement)
Parameters: displacement (float) – New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Normal¶
-
PlaneSearchTermBuilder.
Normal
¶ Returns or sets the normal of the plane.
-------------------------------------
Getter Method
Signature
Normal()
Returns: Return type: NXOpen.Vector3d
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
Normal(normal)
Parameters: normal ( NXOpen.Vector3d
) –New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
PlaneOverlapLogic¶
-
PlaneSearchTermBuilder.
PlaneOverlapLogic
¶ Returns or sets the plane overlap logic.
-------------------------------------
Getter Method
Signature
PlaneOverlapLogic()
Returns: Return type: NXOpen.Assemblies.PlaneSearchTermPlaneOverlapLogicType
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
PlaneOverlapLogic(planeOverlapLogic)
Parameters: planeOverlapLogic ( NXOpen.Assemblies.PlaneSearchTermPlaneOverlapLogicType
) –New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
PointOnPlane¶
-
PlaneSearchTermBuilder.
PointOnPlane
¶ Returns or sets the normal of the plane.
-------------------------------------
Getter Method
Signature
PointOnPlane()
Returns: Return type: NXOpen.Point3d
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
PointOnPlane(pointOnPlane)
Parameters: pointOnPlane ( NXOpen.Point3d
) –New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SearchTermLogic¶
-
PlaneSearchTermBuilder.
SearchTermLogic
¶ Returns or sets the search term logic.
-------------------------------------
Getter Method
Signature
SearchTermLogic()
Returns: Return type: NXOpen.Assemblies.SearchTermSearchTermLogicType
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
SearchTermLogic(searchTermLogic)
Parameters: searchTermLogic ( NXOpen.Assemblies.SearchTermSearchTermLogicType
) –New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
TrueShapeRefinement¶
-
PlaneSearchTermBuilder.
TrueShapeRefinement
¶ Returns or sets the true-shape refinement.
-------------------------------------
Getter Method
Signature
TrueShapeRefinement()
Returns: Return type: bool New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
TrueShapeRefinement(trueShapeRefinement)
Parameters: trueShapeRefinement (bool) – New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Method Detail¶
Validate¶
-
PlaneSearchTermBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.